<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6qp GUI hang | IPU issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1156193#M162187</link>
    <description>&lt;P&gt;I am having the same issue related with a iMX6QP with latest Linux kernel 4.19.144 and Debian Buster (with added Freescale firmware blob). The GUI hangs after 7/8 minutes with OpenGL (glmark2 and Qt 5.11 EGLFS), no matter if I am using the HDMI output or the LVDS output port.&lt;/P&gt;&lt;P&gt;Is there something to check even if I have not Yocto Installed???&lt;/P&gt;&lt;P&gt;The same distribution and software runs fine with iMX6DL processor (it has not the IPU...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gianluca&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2020 10:01:47 GMT</pubDate>
    <dc:creator>gianlucarenzi71</dc:creator>
    <dc:date>2020-09-21T10:01:47Z</dc:date>
    <item>
      <title>imx6qp GUI hang | IPU issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086641#M159291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;setup:&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;We are having a custom board based on imx6qp with 4G DDR. On software side we are using yocto with kernel 4.14.78 and xfce desktop environment. The board is booting successfully and we can observe GUI on HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Issue:&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;On running glmark2 or graphic based application, after few seconds GUI is stuck. But we can still access the board from console and perform read/write operations. Resolution was 1920x1080 on HDMI while running glmark2. We tried reducing the resolution to 640x480, this just delays the issue. Eventually the GUI is stuck with lower resolution as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Query:&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;In kernel we are using imx6qp.dts with all prg and pre nodes enabled, frame buffer node enabled with prefetch. We are using imx6qp-sabreauto.dts as reference. Any checkpoint regarding this issue? Is this a known issue with this kernel or was it later rectified in other version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know if you need additional information&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Arun Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 05:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086641#M159291</guid>
      <dc:creator>arunkumar_ev</dc:creator>
      <dc:date>2020-04-28T05:07:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx6qp GUI hang | IPU issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086642#M159292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what bsp used in the case, may be recommended to try one from nxp&lt;/P&gt;&lt;P&gt;official source.codeaurora.org/external/imx/linux-imx&amp;nbsp; repository&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux L4.14.78_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Try to reproduce issue on i.MX6QP Sabre SD reference board with&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_MX6QDLSOLOX&amp;amp;appType=license&amp;amp;location=null" target="_blank"&gt;Linux Binary Demo Files - i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6SoloX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 08:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086642#M159292</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-04-28T08:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx6qp GUI hang | IPU issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086643#M159293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using yocto sumo release 4.14.78 for imx6 from NXP.&lt;/P&gt;&lt;P&gt;Release manifest - imx_4.14.78_1.0.0_ga.xml&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Arun Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 10:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086643#M159293</guid>
      <dc:creator>arunkumar_ev</dc:creator>
      <dc:date>2020-04-28T10:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: imx6qp GUI hang | IPU issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086644#M159294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to narrow down problem (if it is hardware or software) one can try to reproduce issue on i.MX6QP Sabre SD reference board with&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DL4.14.78_1.0.0_MX6QDLSOLOX%26appType%3Dlicense%26location%3Dnull" rel="nofollow" target="_blank"&gt;Linux Binary Demo Files - i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6SoloX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 13:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1086644#M159294</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-04-28T13:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx6qp GUI hang | IPU issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1156193#M162187</link>
      <description>&lt;P&gt;I am having the same issue related with a iMX6QP with latest Linux kernel 4.19.144 and Debian Buster (with added Freescale firmware blob). The GUI hangs after 7/8 minutes with OpenGL (glmark2 and Qt 5.11 EGLFS), no matter if I am using the HDMI output or the LVDS output port.&lt;/P&gt;&lt;P&gt;Is there something to check even if I have not Yocto Installed???&lt;/P&gt;&lt;P&gt;The same distribution and software runs fine with iMX6DL processor (it has not the IPU...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gianluca&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 10:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-GUI-hang-IPU-issue/m-p/1156193#M162187</guid>
      <dc:creator>gianlucarenzi71</dc:creator>
      <dc:date>2020-09-21T10:01:47Z</dc:date>
    </item>
  </channel>
</rss>