<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP MCU Boot Utility says I have a Non-XIP Application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1155533#M162107</link>
    <description>&lt;P&gt;I am using a IM 1064 board.&lt;/P&gt;&lt;P&gt;I put it in serial download mode (01b).&lt;/P&gt;&lt;P&gt;I am using the UART connection (via USB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to flash the blinky example.&lt;/P&gt;&lt;P&gt;But I get the error &lt;STRONG&gt;"Non-XIP Application is detected but it is not in the range of iTCM/DTCM/OCRAM/SDRAM"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am surprised, I think the binary should be ready to be stored in QSPI and not somehow be marked as "Non-XIP"&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Why does the&amp;nbsp;MCU Boot Utility think I have a Non-XIP Application?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Sep 2020 11:58:25 GMT</pubDate>
    <dc:creator>ruudmeer</dc:creator>
    <dc:date>2020-09-18T11:58:25Z</dc:date>
    <item>
      <title>NXP MCU Boot Utility says I have a Non-XIP Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1155533#M162107</link>
      <description>&lt;P&gt;I am using a IM 1064 board.&lt;/P&gt;&lt;P&gt;I put it in serial download mode (01b).&lt;/P&gt;&lt;P&gt;I am using the UART connection (via USB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to flash the blinky example.&lt;/P&gt;&lt;P&gt;But I get the error &lt;STRONG&gt;"Non-XIP Application is detected but it is not in the range of iTCM/DTCM/OCRAM/SDRAM"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am surprised, I think the binary should be ready to be stored in QSPI and not somehow be marked as "Non-XIP"&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Why does the&amp;nbsp;MCU Boot Utility think I have a Non-XIP Application?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 11:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1155533#M162107</guid>
      <dc:creator>ruudmeer</dc:creator>
      <dc:date>2020-09-18T11:58:25Z</dc:date>
    </item>
    <item>
      <title>Re: NXP MCU Boot Utility says I have a Non-XIP Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1155534#M162108</link>
      <description>&lt;P&gt;Extra info attached&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 12:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1155534#M162108</guid>
      <dc:creator>ruudmeer</dc:creator>
      <dc:date>2020-09-18T12:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: NXP MCU Boot Utility says I have a Non-XIP Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1156140#M162180</link>
      <description>&lt;P&gt;For some reason my files are not loaded correctly.&lt;/P&gt;&lt;P&gt;Here I try again.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 08:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1156140#M162180</guid>
      <dc:creator>ruudmeer</dc:creator>
      <dc:date>2020-09-21T08:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: NXP MCU Boot Utility says I have a Non-XIP Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1156416#M162216</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;I am unable to open your files, it seems that there is a reported issue with attachments at the moment and our team is working on getting this fixed with #1 priority. For the time being I'd like to review the steps you took to get this up and running so I can check if something was missed. Did you follow the steps in the &lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_self"&gt;github page&lt;/A&gt; for the mcu boot utility tool?&lt;/P&gt;
&lt;P&gt;If so, please check the section 2, where it explains a part of the led-blink as a non-xip image and the modifications to be made.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have questions.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 17:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-MCU-Boot-Utility-says-I-have-a-Non-XIP-Application/m-p/1156416#M162216</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-21T17:31:35Z</dc:date>
    </item>
  </channel>
</rss>