<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6dual PCIE Function application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6dual-PCIE-Function-application/m-p/1155528#M162105</link>
    <description>&lt;P&gt;1. Any kind of data, including video, can be transferred over a PCIe link.&lt;/P&gt;
&lt;P&gt;2. Yes, the PCIe controller of i.MX6Dual can operate as either Root Complex or Endpoint.&lt;/P&gt;
&lt;P&gt;3. The i.MX6Dual PCIe interface conforms to the PCIe v.2.0 specification that provides 5Gbit/s data throughput.&lt;/P&gt;
&lt;P&gt;4. The Linux BSP contains the PCIe driver. For details, please refer to the corresponding chapter of the i.MX Linux Reference Manual document:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Fri, 18 Sep 2020 11:42:01 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2020-09-18T11:42:01Z</dc:date>
    <item>
      <title>I.MX6dual PCIE Function application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6dual-PCIE-Function-application/m-p/1150938#M161501</link>
      <description>&lt;P&gt;1、PCIE interface supports video transmission?&lt;/P&gt;&lt;P&gt;2、Does PCIE support master-slave Settings?&lt;/P&gt;&lt;P&gt;3、What is the maximum rate supported by PCIE?&lt;/P&gt;&lt;P&gt;4、What functions does the underlying software PCIE currently support?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 07:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6dual-PCIE-Function-application/m-p/1150938#M161501</guid>
      <dc:creator>tommyduan</dc:creator>
      <dc:date>2020-09-09T07:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6dual PCIE Function application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6dual-PCIE-Function-application/m-p/1155528#M162105</link>
      <description>&lt;P&gt;1. Any kind of data, including video, can be transferred over a PCIe link.&lt;/P&gt;
&lt;P&gt;2. Yes, the PCIe controller of i.MX6Dual can operate as either Root Complex or Endpoint.&lt;/P&gt;
&lt;P&gt;3. The i.MX6Dual PCIe interface conforms to the PCIe v.2.0 specification that provides 5Gbit/s data throughput.&lt;/P&gt;
&lt;P&gt;4. The Linux BSP contains the PCIe driver. For details, please refer to the corresponding chapter of the i.MX Linux Reference Manual document:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 11:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6dual-PCIE-Function-application/m-p/1155528#M162105</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2020-09-18T11:42:01Z</dc:date>
    </item>
  </channel>
</rss>