<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: pf0100f9azes in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155320#M162076</link>
    <description>&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;I assembled three boards, one outpiu voltage is OK except 1.2V, which I don't need it, the other two have the same issue and the voltage are the same, 2.3V and 2.8V, instead of 1.5V&amp;nbsp; and 1.8V. included is the schemmatics.&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="systemPower.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125556i2FF37C195FE55647/image-size/large?v=v2&amp;amp;px=999" role="button" title="systemPower.jpg" alt="systemPower.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;systemPower.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Sep 2020 07:00:19 GMT</pubDate>
    <dc:creator>hailiu</dc:creator>
    <dc:date>2020-09-18T07:00:19Z</dc:date>
    <item>
      <title>pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1154454#M161962</link>
      <description>&lt;P&gt;I used PF0100F9AZES PMIC to generate system power, one board generate all the correct power, the other one has some issues. According to the spec, Vgen2 pin 18) should generate a 1.5V output, but I get a 2.8V output, sw4LX (pin 21), after the inductor, I should get a 1.8V output, but I get a 2.4V output? some things wrong? or the chip was not programmed correctly?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 03:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1154454#M161962</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2020-09-17T03:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1154465#M161965</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/118084"&gt;@hailiu&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is it possible to look at schematic?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 04:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1154465#M161965</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-09-17T04:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155320#M162076</link>
      <description>&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;I assembled three boards, one outpiu voltage is OK except 1.2V, which I don't need it, the other two have the same issue and the voltage are the same, 2.3V and 2.8V, instead of 1.5V&amp;nbsp; and 1.8V. included is the schemmatics.&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="systemPower.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125556i2FF37C195FE55647/image-size/large?v=v2&amp;amp;px=999" role="button" title="systemPower.jpg" alt="systemPower.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;systemPower.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 07:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155320#M162076</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2020-09-18T07:00:19Z</dc:date>
    </item>
    <item>
      <title>Re: pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155345#M162080</link>
      <description>&lt;P&gt;vgen1 (pin 16) are 0V for all three boards.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 07:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155345#M162080</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2020-09-18T07:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155351#M162082</link>
      <description>&lt;P&gt;I guess that because the output of pin 21 (SW4LX) is 2.4V, the input to pin 17 is 2.4V, that's cause the output of Vgen2 is high. I checked the inputs on pin 7,10,12, there are all 4.36V, it seems a reasonable value, the problem is why output of sw4 is high?&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 08:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155351#M162082</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2020-09-18T08:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: pf0100f9azes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155601#M162123</link>
      <description>&lt;P&gt;Found the problem. Not the pmic problem, but the output pin was shorted to a 3.0v trace.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 14:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pf0100f9azes/m-p/1155601#M162123</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2020-09-18T14:22:07Z</dc:date>
    </item>
  </channel>
</rss>