<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8M Mini Storage Temperature</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153553#M161849</link>
    <description>&lt;P&gt;The temperature spec for storage for the i.MX8M Mini is -40C to 150C.&amp;nbsp; Can the processor be stored (without power) at lower temps without damage?&amp;nbsp; I wasn't sure if the -40C is specified because:&lt;/P&gt;&lt;P&gt;-It is related with the industrial operating temp range (-40/85C) and the measurement wasn't required or made any lower&amp;nbsp; OR&lt;/P&gt;&lt;P&gt;-Something within the package could be damaged if taken that low even in storage (without power).&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2020 14:55:43 GMT</pubDate>
    <dc:creator>rfguy1</dc:creator>
    <dc:date>2020-09-15T14:55:43Z</dc:date>
    <item>
      <title>i.MX8M Mini Storage Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153553#M161849</link>
      <description>&lt;P&gt;The temperature spec for storage for the i.MX8M Mini is -40C to 150C.&amp;nbsp; Can the processor be stored (without power) at lower temps without damage?&amp;nbsp; I wasn't sure if the -40C is specified because:&lt;/P&gt;&lt;P&gt;-It is related with the industrial operating temp range (-40/85C) and the measurement wasn't required or made any lower&amp;nbsp; OR&lt;/P&gt;&lt;P&gt;-Something within the package could be damaged if taken that low even in storage (without power).&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 14:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153553#M161849</guid>
      <dc:creator>rfguy1</dc:creator>
      <dc:date>2020-09-15T14:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini Storage Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153555#M161851</link>
      <description>&lt;P&gt;Failed to mention the interest is to -55C.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 14:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153555#M161851</guid>
      <dc:creator>rfguy1</dc:creator>
      <dc:date>2020-09-15T14:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini Storage Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153901#M161898</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178005"&gt;@rfguy1&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You are right - the storage temperature must not be lower, than -40 C, since&lt;BR /&gt;"something within the package could be damaged if taken that low even in storage (without power)."&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 06:38:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Storage-Temperature/m-p/1153901#M161898</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-09-16T06:38:30Z</dc:date>
    </item>
  </channel>
</rss>