<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6SLL + IMXEBOOKDC4: Change EPDC resolution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152353#M161683</link>
    <description>&lt;P&gt;This is the console&lt;/P&gt;&lt;P&gt;xres and yres are not aligned to the panel resolution&lt;/P&gt;&lt;P&gt;mxc_epdc_fb_test.out crashes at Blank Screen&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;root@imx6sllevk:/unit_tests/Display# ./mxc_epdc_fb_test.out&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;---- Running &amp;lt; ./mxc_epdc_fb_test.out &amp;gt; test ----&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;Opened EPDC fb device /dev/fb2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set the background to 16-bpp&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.xres_virtual = 1024&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.yres_virtual = 1536&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.bits_per_pixel = 16&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Mem-Mapping FB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set to region update mode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set waveform modes&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set update scheme - 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set pwrdown_delay - 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Blank screen&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;���&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 10:00:05 +0000)&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;CPU: Freescale i.MX6SLL rev1.1 996 MHz (running at 792 MHz)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Commercial temperature grade (0C to 95C) at 36C&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: POR&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Model: Freescale i.MX6SLL EVK Board&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: MX6SLL EVK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 2 GiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading Environment from MMC... OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;No panel detected: default to MCIMX28LCD&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Display: MCIMX28LCD (800x480)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Video: 800x480x24&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 12 Sep 2020 00:56:23 GMT</pubDate>
    <dc:creator>ekerebel</dc:creator>
    <dc:date>2020-09-12T00:56:23Z</dc:date>
    <item>
      <title>IMX6SLL + IMXEBOOKDC4: Change EPDC resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152326#M161681</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I received a new panel from EINK (ED060KG2) that I want to test with my IMX6SLL Dev Board + IMXEBOOKDC4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have loaded the .fw that I have received from NXP and entered the following config in UBOOT:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;&lt;SPAN&gt;setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:ED060KG2C1,bpp=16 max17135:pass=2,vcom=-2560000&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The ED060KG2 is a 1440x1072 EPD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When I launch the test program, the board crashes and reboots.&lt;/P&gt;&lt;P&gt;The framebuffer still indicates a 1024x758 resolution:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;root@imx6sllevk:~# fbset -fb /dev/fb2&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;mode "1024x758-0"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;# &lt;LI-EMOJI id="lia_anguished-face" title=":anguished_face:"&gt;&lt;/LI-EMOJI&gt; 0.025 MHz, H: 0.022 kHz, V: 0.029 Hz&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;geometry 1024 758 1024 1536 16&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;timings 40000000 12 76 4 5 12 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;accel false&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;rgba 5/11,6/5,5/0,0/0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;endmode&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;When I try to set the resolution of /dev/fb2, the system crashes and reboots.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the provided SDCard with the dev board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 21:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152326#M161681</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2020-09-11T21:58:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SLL + IMXEBOOKDC4: Change EPDC resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152353#M161683</link>
      <description>&lt;P&gt;This is the console&lt;/P&gt;&lt;P&gt;xres and yres are not aligned to the panel resolution&lt;/P&gt;&lt;P&gt;mxc_epdc_fb_test.out crashes at Blank Screen&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;root@imx6sllevk:/unit_tests/Display# ./mxc_epdc_fb_test.out&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;---- Running &amp;lt; ./mxc_epdc_fb_test.out &amp;gt; test ----&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;Opened EPDC fb device /dev/fb2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set the background to 16-bpp&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.xres_virtual = 1024&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.yres_virtual = 1536&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;screen_info.bits_per_pixel = 16&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Mem-Mapping FB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set to region update mode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set waveform modes&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set update scheme - 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Set pwrdown_delay - 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Blank screen&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;���&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 10:00:05 +0000)&lt;/EM&gt;&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;CPU: Freescale i.MX6SLL rev1.1 996 MHz (running at 792 MHz)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Commercial temperature grade (0C to 95C) at 36C&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: POR&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Model: Freescale i.MX6SLL EVK Board&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: MX6SLL EVK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 2 GiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading Environment from MMC... OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;No panel detected: default to MCIMX28LCD&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Display: MCIMX28LCD (800x480)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Video: 800x480x24&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 12 Sep 2020 00:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152353#M161683</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2020-09-12T00:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SLL + IMXEBOOKDC4: Change EPDC resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152419#M161694</link>
      <description>&lt;P&gt;Disregard my question, I had 2 issues:&lt;/P&gt;&lt;P&gt;1- powering through USB instead of 5V probably caused the crash&lt;/P&gt;&lt;P&gt;2- I had to recompile the mxc_epdc_v2_fb.c in the kernel with a new panel resolution&lt;/P&gt;</description>
      <pubDate>Sat, 12 Sep 2020 21:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLL-IMXEBOOKDC4-Change-EPDC-resolution/m-p/1152419#M161694</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2020-09-12T21:30:16Z</dc:date>
    </item>
  </channel>
</rss>