<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: about non-branching problem from ROM code boot to u-boot image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1150014#M161381</link>
    <description>&lt;P&gt;During use "uuu -b emmc files\u-boot-imx6solo.imx" to write u-boot to eMMC, debug UART will output booting logs on console. If you can see the logs, it means your DDR is no problem, the u-boot should noramlly boot your board.&lt;/P&gt;
&lt;P&gt;But if you can't see logs on console during programming u-boot to eMMC, probably there still exist some issues with the u-boot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a&amp;nbsp; nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2020 03:44:41 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2020-09-08T03:44:41Z</dc:date>
    <item>
      <title>about non-branching problem from ROM code boot to u-boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133444#M160954</link>
      <description>&lt;P&gt;hi.&lt;/P&gt;&lt;P&gt;I downloaded the binary using uuu on i.MX6Solo's eMMC (dev:2). (This board is made by referring to PCB of I.MX6Q SabreSD.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then, The BOOT_CFG was changed to eMMC and booted, but, u-boot message was not printed on the terminal.&lt;/P&gt;&lt;P&gt;And, after a certain period of time, it changes to serial download mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BOOT_CFG was also set as eMMC, and the binary was downloaded to eMMC, but what is the cause of the phenomenon that does not boot from ROM BOOT to u-boot?&lt;/P&gt;&lt;P&gt;(The eMMC checked the normal boot at the prompt of u-boot in serial download mode and confirmed that u-boot with dump : Attached files are mmcblk3boot0 and mmcblk3boot1. mmcblk3 attached a file with only the front part dump.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please review.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 01:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133444#M160954</guid>
      <dc:creator>donghyunkim</dc:creator>
      <dc:date>2020-09-02T01:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: about non-branching problem from ROM code boot to u-boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133579#M160963</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; if the PMIC+CPU+DDR+eMMC(sd) is the same as those of i.MX6Q SDB, you can use "uuu -b emmc u-boot-imx" to program images to board after compiling linux bsp of&amp;nbsp; i.MX6Q SabreSDB&lt;/P&gt;
&lt;P&gt;Then try to boot it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; If u-boot can boot your board, please use imx6 / 7 ddr stress test tool to do calibration and stress test, then change ddr configurations according to prompt from calibration.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; Then write u-boot to eMMC again....&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 03:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133579#M160963</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-09-02T03:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: about non-branching problem from ROM code boot to u-boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133629#M160968</link>
      <description>&lt;P&gt;hi, weidong&lt;/P&gt;&lt;P&gt;I tried "uuu -b emmc u-boot-imx" but it &lt;FONT color="#FF0000"&gt;doesn't boot up.&lt;/FONT&gt;&lt;BR /&gt;u-boot has been written to eMMC.&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="100%"&gt;&lt;P&gt;C:\uuu&amp;gt;uuu -b emmc files\u-boot-imx6solo.imx&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.191-0-g4fe24b9&lt;/P&gt;&lt;P&gt;Success 1 Failure 0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;3:96 7/ 7 [Done ] FB: Done&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What are the cases where i can not jump from ROM boot to u-boot?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 04:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1133629#M160968</guid>
      <dc:creator>donghyunkim</dc:creator>
      <dc:date>2020-09-02T04:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: about non-branching problem from ROM code boot to u-boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1134775#M161028</link>
      <description>&lt;P&gt;hi, weidong.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There seems to be no problem with the DDR test.&lt;BR /&gt;I attached the log file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 01:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1134775#M161028</guid>
      <dc:creator>donghyunkim</dc:creator>
      <dc:date>2020-09-03T01:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: about non-branching problem from ROM code boot to u-boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1150014#M161381</link>
      <description>&lt;P&gt;During use "uuu -b emmc files\u-boot-imx6solo.imx" to write u-boot to eMMC, debug UART will output booting logs on console. If you can see the logs, it means your DDR is no problem, the u-boot should noramlly boot your board.&lt;/P&gt;
&lt;P&gt;But if you can't see logs on console during programming u-boot to eMMC, probably there still exist some issues with the u-boot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a&amp;nbsp; nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 03:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-non-branching-problem-from-ROM-code-boot-to-u-boot-image/m-p/1150014#M161381</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-09-08T03:44:41Z</dc:date>
    </item>
  </channel>
</rss>