<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx-atf boot flow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-atf-boot-flow/m-p/1149761#M161347</link>
    <description>&lt;P&gt;Yes, this is supported, but it has never implemented from our side&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 07 Sep 2020 14:43:23 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2020-09-07T14:43:23Z</dc:date>
    <item>
      <title>imx-atf boot flow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-atf-boot-flow/m-p/1069875#M157160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git/tree/docs/design/firmware-design.rst?h=v2.3"&gt;imx-atf&lt;/A&gt; allows alternative boot flow by preloading a BL33 (custom) image into memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any instructions on how to use BL2 to boot an EL3 payload for pre-production test work ? Can we use EL3_PAYLOAD_BASE option ? Can someone point to some example instructions/app notes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, there is the FIP build command "&lt;SPAN style="font-family: 'courier new', courier, monospace;"&gt;make PRELOADED_BL33_BASE=0x80000000 PLAT=imx8qm all fip&lt;/SPAN&gt;". Does i.MX8QM plaform support this? Can it be used to allow booting a custom image (like Linux kernel or some app) from TF-A ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 19:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-atf-boot-flow/m-p/1069875#M157160</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2020-08-26T19:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx-atf boot flow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-atf-boot-flow/m-p/1149761#M161347</link>
      <description>&lt;P&gt;Yes, this is supported, but it has never implemented from our side&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 14:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-atf-boot-flow/m-p/1149761#M161347</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2020-09-07T14:43:23Z</dc:date>
    </item>
  </channel>
</rss>