<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx8qxpc0mek - Yocto Linux BSP issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1149526#M161307</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;On iMX8QuadXPlus (C0 MEK) board, I have compiled and flashed the Yocto-Linux Binary (made from 'imx-yocto-L5.4.24_2.1.0').&lt;/P&gt;&lt;P&gt;I'm facing some of the following issues.&lt;/P&gt;&lt;P&gt;1) 'sudo apt-get install' commands throw the following error.&lt;/P&gt;&lt;P&gt;apt-get: error while loading shared libraries: libgcc_s.so.1: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;(However, the libgcc_s.so.1 file is present at '/lib/aarch64-linux-gnu/' already.)&lt;/P&gt;&lt;P&gt;2) Following LoadLocale error is occurring while executing any application.&lt;/P&gt;&lt;P&gt;loadlocale.c:129: _nl_intern_locale_data: Assertion `cnt &amp;lt; (sizeof (_nl_value_type_LC_TIME) / sizeof (_nl_value_type_LC_TIME[0]))' failed.&lt;/P&gt;&lt;P&gt;Please inform if any patch/bugfix available for resolving the above mentioned errors.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Sep 2020 07:42:21 GMT</pubDate>
    <dc:creator>arunkumarjts</dc:creator>
    <dc:date>2020-09-07T07:42:21Z</dc:date>
    <item>
      <title>imx8qxpc0mek - Yocto Linux BSP issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1149526#M161307</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;On iMX8QuadXPlus (C0 MEK) board, I have compiled and flashed the Yocto-Linux Binary (made from 'imx-yocto-L5.4.24_2.1.0').&lt;/P&gt;&lt;P&gt;I'm facing some of the following issues.&lt;/P&gt;&lt;P&gt;1) 'sudo apt-get install' commands throw the following error.&lt;/P&gt;&lt;P&gt;apt-get: error while loading shared libraries: libgcc_s.so.1: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;(However, the libgcc_s.so.1 file is present at '/lib/aarch64-linux-gnu/' already.)&lt;/P&gt;&lt;P&gt;2) Following LoadLocale error is occurring while executing any application.&lt;/P&gt;&lt;P&gt;loadlocale.c:129: _nl_intern_locale_data: Assertion `cnt &amp;lt; (sizeof (_nl_value_type_LC_TIME) / sizeof (_nl_value_type_LC_TIME[0]))' failed.&lt;/P&gt;&lt;P&gt;Please inform if any patch/bugfix available for resolving the above mentioned errors.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 07:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1149526#M161307</guid>
      <dc:creator>arunkumarjts</dc:creator>
      <dc:date>2020-09-07T07:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxpc0mek - Yocto Linux BSP issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1149576#M161313</link>
      <description>&lt;P&gt;Hi&amp;nbsp;arunkumarjts&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;these commands are used in debian so one can try below guidelines:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://boundarydevices.com/customizing-ubuntu-debian-kernels-on-i-mx8-boards/" target="_blank"&gt;https://boundarydevices.com/customizing-ubuntu-debian-kernels-on-i-mx8-boards/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Build-Ubuntu-For-i-MX8-Series-Platform/ta-p/1128708" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Build-Ubuntu-For-i-MX8-Series-Platform/ta-p/1128708&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 08:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1149576#M161313</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-07T08:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxpc0mek - Yocto Linux BSP issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1152451#M161697</link>
      <description>&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;On the imx8-QuadXPlus - c0 - MEK board, I have replaced the binary with 'L4.14.98_2.0.0' (Yocto-Linux) BSP.&lt;/P&gt;&lt;P&gt;The board is booting fine and found that &lt;STRONG&gt;dnf&lt;/STRONG&gt; built-in package manager is present in it.&lt;/P&gt;&lt;P&gt;However, while doing the upgrade or install any package through the '&lt;STRONG&gt;dnf&lt;/STRONG&gt;' , it says, 'Error: There are no enabled repos.'.&lt;/P&gt;&lt;P&gt;I could not add the repos using the 'dnf config-manager --add-repo &lt;A href="http://springdale.math.ias.edu/data/puias/unsupported/7/x86_64/" target="_blank"&gt;http://springdale.math.ias.edu/data/puias/unsupported/7/x86_64/&lt;/A&gt;' command also. It says, 'No such command: config-manager. Please use /usr/bin/dnf --help'&lt;/P&gt;&lt;P&gt;Kindly inform, how to activate the repos for using the '&lt;STRONG&gt;dnf&lt;/STRONG&gt;'.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;</description>
      <pubDate>Sun, 13 Sep 2020 08:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxpc0mek-Yocto-Linux-BSP-issues/m-p/1152451#M161697</guid>
      <dc:creator>arunkumarjts</dc:creator>
      <dc:date>2020-09-13T08:10:20Z</dc:date>
    </item>
  </channel>
</rss>