<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 Quad Local Timer</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1149329#M161284</link>
    <description>&lt;P&gt;For anyone following this and doing a bare metal application, the above interrupt vectors are wrong. The Reset, Undefined, SVC, Prefetch, Data Abort, IRQ, and FIQ interrupts are vectored by the VBR. GIC vectors are as follows:&lt;/P&gt;&lt;P&gt;0 - 16&amp;nbsp; &amp;nbsp; Software generated interrupts&lt;/P&gt;&lt;P&gt;16 - 26&amp;nbsp; Not used&lt;/P&gt;&lt;P&gt;27, 28&amp;nbsp; &amp;nbsp;Not sure&lt;/P&gt;&lt;P&gt;29&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Local timer&lt;/P&gt;&lt;P&gt;30, 31&amp;nbsp; &amp;nbsp;Not sure&lt;/P&gt;&lt;P&gt;32 - 159&amp;nbsp; &amp;nbsp;See Table 3-1 in the RM (as of Rev 5, 6/18)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The base address of the local timer is in fact 0x00A00600. The register set for controlling it as given above are correct. The bit definitions in the Control Register are:&lt;/P&gt;&lt;P&gt;// Bit definitions for the Control Register&lt;BR /&gt;#define LOCTMR_CNTL_TMRENB 0x00000001 //timer enable&lt;BR /&gt;#define LOCTMR_CNTL_AUTORL 0x00000002 //auto reload&lt;BR /&gt;#define LOCTMR_CNTL_IRQENB 0x00000004 //interrupt enable&lt;BR /&gt;#define LOCTMR_CNTL_PRESCL_MASK 0x0000FF00 //controller prescaler mask&lt;/P&gt;&lt;P&gt;Note that the counter as is is a down counter. Does anyone know if there is a bit in the Control Register to change to an up counter?&lt;/P&gt;</description>
    <pubDate>Sun, 06 Sep 2020 23:30:45 GMT</pubDate>
    <dc:creator>ogj</dc:creator>
    <dc:date>2020-09-06T23:30:45Z</dc:date>
    <item>
      <title>iMX6 Quad Local Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073116#M157596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the local timer in one of the cores to create a "tick" timer. According to what I've read in various manuals, each of the cores in the iMX6 Quad has a private timer that can be used for my application. My understanding is that each of these timers will have the same bus address (for ease of SW)&amp;nbsp; but the timer will only respond to the core it belongs to; kind of like a private address within the core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is that there is not a lot of information about these timers. I believe that the address of the timer starts at 0x00A00600 - is this correct? I believe the register structure is: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;// LOCTMR - Peripheral register structure&lt;BR /&gt;typedef struct LOCTMR_MemMap&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; uint32_t LDVAL;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //counter reload value&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; offset 0x000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; uint32_t CNTR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //count reg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; offset 0x004&lt;BR /&gt;&amp;nbsp;&amp;nbsp; uint32_t CNTL;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //control reg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; offset 0x008&lt;BR /&gt;&amp;nbsp;&amp;nbsp; uint32_t INTSTS;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //interrupt status reg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; offset 0x00C&lt;BR /&gt;} volatile *LOCTMR_MemMapPtr;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the above information correct? I have been unable to find what the interrupt vector is - where do I find it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 05:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073116#M157596</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-05-26T05:26:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Quad Local Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073117#M157597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i.MX6 Reference Manual (RM) in Table 2-1 (System memory map) provides address section&lt;/P&gt;&lt;P&gt;from 0x00A0_0000 till&amp;nbsp; 0x00A0_1FFF&amp;nbsp; for&amp;nbsp; ARM MP resources, where Global and Private &lt;BR /&gt;timers may be found. Use ARM documentation for more details about the timers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407e/CIHJGFEA.html" title="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407e/CIHJGFEA.html"&gt;ARM Information Center&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; According to section 3.2 (Cortex A9 interrupts) of the i.MX6 RM:&lt;BR /&gt;&lt;EM&gt;"The Global Interrupt Controller (GIC) collects up to 128 interrupt requests from all chip&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sources and provides an interface to the Cortex A9 CPU cores. The first 32 interrupts are&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;private to the CPUs' interface. These interrupts are not included in the table below. All&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;interrupts besides those private to the CPU are hooked up to the GPC."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 06:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073117#M157597</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-05-26T06:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Quad Local Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073118#M157598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I saw Table 2-1, that's where I got the 0x00A00600 from. However the entry for Table 2-1 for the range 00A0_0000 to 00A0_1FFF says private timers and watchdogs, so there's more than just one timer in there. What's the address of the local timer? Also I know that the first 32 interrupts are private to each of the cores. Here's what I know so far:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;// GIC Interrupt Number Definitions&lt;BR /&gt;typedef enum&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reset&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reset (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_UndefinedInstruction&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 1,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Undefined Instruction (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_SupervisorCall&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 2,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Supervisor Call (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_PrefetchAbort&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 3,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Prefetch Abort (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_DataAbort&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Data Abort (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved5&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 5,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_IRQ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 6,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IRQ (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_FIRQ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 7,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Fast IRQ (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 8,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved9&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 9,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved10&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 10,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved11&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 11,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved12&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 12,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved13&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 13,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved14&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 14,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; A9_Reserved15&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 15,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reserved (Hardware Interrupt)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 16,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 17,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 18,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 19,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 20,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI5&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 21,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI6&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 22,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI7&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 23,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 24,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI9&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 25,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI10&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 26,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI11&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 27,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI12&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 28,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI13&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 29,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI14&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 30,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SGI15&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 31,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Software Generated Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_IOMUXC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 32,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Private Peripheral Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_DAP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 33,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Private Peripheral Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SDMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 34,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Private Peripheral Interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_VPU_JPG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 35,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // JPEG codec interrupt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_SVNS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 36,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PMIC power off request&lt;BR /&gt;&amp;nbsp;&amp;nbsp; GIC_IPU&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 37,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // IPU error interrupt&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I figure that the timer interrupt is between 8-15 but which one? I'd also like to verify that my understanding of the local timer register set is correct. Anyone know?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 15:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073118#M157598</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-05-26T15:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Quad Local Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073119#M157599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone have an answer to what is the address of the register set for the local timer and what is the interrupt vector?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 13:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1073119#M157599</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-06-04T13:50:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Quad Local Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1149329#M161284</link>
      <description>&lt;P&gt;For anyone following this and doing a bare metal application, the above interrupt vectors are wrong. The Reset, Undefined, SVC, Prefetch, Data Abort, IRQ, and FIQ interrupts are vectored by the VBR. GIC vectors are as follows:&lt;/P&gt;&lt;P&gt;0 - 16&amp;nbsp; &amp;nbsp; Software generated interrupts&lt;/P&gt;&lt;P&gt;16 - 26&amp;nbsp; Not used&lt;/P&gt;&lt;P&gt;27, 28&amp;nbsp; &amp;nbsp;Not sure&lt;/P&gt;&lt;P&gt;29&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Local timer&lt;/P&gt;&lt;P&gt;30, 31&amp;nbsp; &amp;nbsp;Not sure&lt;/P&gt;&lt;P&gt;32 - 159&amp;nbsp; &amp;nbsp;See Table 3-1 in the RM (as of Rev 5, 6/18)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The base address of the local timer is in fact 0x00A00600. The register set for controlling it as given above are correct. The bit definitions in the Control Register are:&lt;/P&gt;&lt;P&gt;// Bit definitions for the Control Register&lt;BR /&gt;#define LOCTMR_CNTL_TMRENB 0x00000001 //timer enable&lt;BR /&gt;#define LOCTMR_CNTL_AUTORL 0x00000002 //auto reload&lt;BR /&gt;#define LOCTMR_CNTL_IRQENB 0x00000004 //interrupt enable&lt;BR /&gt;#define LOCTMR_CNTL_PRESCL_MASK 0x0000FF00 //controller prescaler mask&lt;/P&gt;&lt;P&gt;Note that the counter as is is a down counter. Does anyone know if there is a bit in the Control Register to change to an up counter?&lt;/P&gt;</description>
      <pubDate>Sun, 06 Sep 2020 23:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Quad-Local-Timer/m-p/1149329#M161284</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-09-06T23:30:45Z</dc:date>
    </item>
  </channel>
</rss>