<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックThis an automatic process.  We are marking this post as s...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/1136652#M161170</link>
    <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
    <pubDate>Thu, 03 Sep 2020 16:15:06 GMT</pubDate>
    <dc:creator>CommunityBot</dc:creator>
    <dc:date>2020-09-03T16:15:06Z</dc:date>
    <item>
      <title>EIM: Muxed 16-bit NOR Flash Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/380046#M54739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Champs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A customer is asking for schematics or diagrams which use a 16-bit multiplexed NOR Flash connected to EIM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found some of SPI NOR Flash cases but none of EIM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please introduce if there is any.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nori Shinozaki &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 04:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/380046#M54739</guid>
      <dc:creator>norishinozaki</dc:creator>
      <dc:date>2015-03-12T04:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: EIM: Muxed 16-bit NOR Flash Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/380047#M54740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nori&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think below diagram may be useful&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51290i837EBA150670E94D/image-size/large?v=v2&amp;amp;px=999" title="Muxed Mode.jpg" alt="Muxed Mode.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 04:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/380047#M54740</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-12T04:49:10Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/1136652#M161170</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 16:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Muxed-16-bit-NOR-Flash-Example/m-p/1136652#M161170</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T16:15:06Z</dc:date>
    </item>
  </channel>
</rss>