<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックThis an automatic process.  We are marking this post as s...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/1135919#M161123</link>
    <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
    <pubDate>Thu, 03 Sep 2020 14:59:46 GMT</pubDate>
    <dc:creator>CommunityBot</dc:creator>
    <dc:date>2020-09-03T14:59:46Z</dc:date>
    <item>
      <title>I.MX6Q  PCM Bluetooth?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/343146#M47217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;Now,I want to use bluetooth on I.MX6Q_SABRESD.&lt;/P&gt;&lt;P&gt;My BSP is linux-3.0.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there pcm BT functions on imx6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thaks a lot !&lt;/P&gt;&lt;P&gt;Chen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 03:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/343146#M47217</guid>
      <dc:creator>ct3paul</dc:creator>
      <dc:date>2015-03-24T03:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6Q  PCM Bluetooth?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/343147#M47218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6Q processor itself does not contain any specific Bluetooth-related functions. However, it contains a number of digital audio interfaces (SSI, ESAI) that can handle an external PCM audio devices. The Linux 3.0.35 BSP contains the Bluetooth driver that can handle A2DP and AVRCP profiles. For more information, please refer to the Chapter 41 of the i.MX 6Dual/Quad Linux Reference Manual document, available as the part of the L3.0.35_4.1.0_LINUX_DOCS documentation bundle on the Freescale web site:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 10:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/343147#M47218</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-03-24T10:33:21Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/1135919#M161123</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 14:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-PCM-Bluetooth/m-p/1135919#M161123</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T14:59:46Z</dc:date>
    </item>
  </channel>
</rss>