<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic This an automatic process.  We are marking this post as s... in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/1135813#M161113</link>
    <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
    <pubDate>Thu, 03 Sep 2020 14:52:57 GMT</pubDate>
    <dc:creator>CommunityBot</dc:creator>
    <dc:date>2020-09-03T14:52:57Z</dc:date>
    <item>
      <title>DDR3 Bit Swaaping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338580#M46263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We swapped the DDR3 bits as recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to map these bits to processor while initializing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 04:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338580#M46263</guid>
      <dc:creator>muralikrishna</dc:creator>
      <dc:date>2015-03-23T04:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Bit Swaaping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338581#M46264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is no need for additional mapping or software reconfiguration, as&lt;/P&gt;&lt;P&gt;it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines &lt;A href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQ6SDLHDG&lt;/A&gt; also&lt;/P&gt;&lt;P&gt;below part of p.4 SPF-27392 Sabre Schematic &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50694i073EC4E717F792BF/image-size/large?v=v2&amp;amp;px=999" title="SPF-27392   p.4.jpg" alt="SPF-27392   p.4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 10:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338581#M46264</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-23T10:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Bit Swaaping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338582#M46265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bit swapping in Hardware is taken care.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to implement those bit swappings in software to write or read to DDR3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Murali&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 10:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338582#M46265</guid>
      <dc:creator>muralikrishna</dc:creator>
      <dc:date>2015-03-23T10:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Bit Swaaping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338583#M46266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general it is not possible to implement bit swappings in software.&lt;/P&gt;&lt;P&gt;If you followed Freescale recommmendations, there is no need &lt;/P&gt;&lt;P&gt;for additional mapping or software reconfiguration,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 10:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338583#M46266</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-23T10:32:35Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Bit Swaaping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338584#M46267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, when swapping the byte lanes, don't forget to route correctly the strobe and mask signals, i.e. DQMx, DQSx and DQSx_B, corresponding to these byte lanes.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 11:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/338584#M46267</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-03-23T11:54:56Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/1135813#M161113</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 14:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Bit-Swaaping/m-p/1135813#M161113</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T14:52:57Z</dc:date>
    </item>
  </channel>
</rss>