<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMfgtool 2.0 (UTP) corrupting image data while loading during bootstrap mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-2-0-UTP-corrupting-image-data-while-loading-during/m-p/1135051#M161058</link>
    <description>&lt;P&gt;We are planning to use Mfgtool 2.0 for manufacturing purposes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing issues in using Mfgtool 2.0 which uses UTP protocol. I downloaded it from the NXP Website.&lt;/P&gt;&lt;P&gt;In the Bootstrap phase, mfgtool is supposed to enable loading of zImage, DTB and rootfs after u-boot.&lt;/P&gt;&lt;P&gt;I can see the u-boot is coming up, but after that I see issues with the DTB and the boot stops. The DTB is supposed to be loaded at the location 0x1800 0000. When I check the contents at the location 0x1800 0000 using "md" command of u-boot, I can see that the first word is corrupted. Rest of the words are correct.&lt;/P&gt;&lt;P&gt;The first word for DTB should be 0xd00dfeed. However, I see it is 0xaa0dfeed in the memory. I can see similar issue with the zImage. For some reason, there is presence of 0xaa in the first word and it causing issue. The Mfgtool is &lt;U&gt;not&lt;/U&gt; able to go beyond the Bootstrap phase.&lt;/P&gt;&lt;P&gt;Did anybody come across the issue? How can this be resolved?&lt;/P&gt;</description>
    <pubDate>Thu, 03 Sep 2020 08:21:35 GMT</pubDate>
    <dc:creator>arindamroy</dc:creator>
    <dc:date>2020-09-03T08:21:35Z</dc:date>
    <item>
      <title>Mfgtool 2.0 (UTP) corrupting image data while loading during bootstrap mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-2-0-UTP-corrupting-image-data-while-loading-during/m-p/1135051#M161058</link>
      <description>&lt;P&gt;We are planning to use Mfgtool 2.0 for manufacturing purposes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing issues in using Mfgtool 2.0 which uses UTP protocol. I downloaded it from the NXP Website.&lt;/P&gt;&lt;P&gt;In the Bootstrap phase, mfgtool is supposed to enable loading of zImage, DTB and rootfs after u-boot.&lt;/P&gt;&lt;P&gt;I can see the u-boot is coming up, but after that I see issues with the DTB and the boot stops. The DTB is supposed to be loaded at the location 0x1800 0000. When I check the contents at the location 0x1800 0000 using "md" command of u-boot, I can see that the first word is corrupted. Rest of the words are correct.&lt;/P&gt;&lt;P&gt;The first word for DTB should be 0xd00dfeed. However, I see it is 0xaa0dfeed in the memory. I can see similar issue with the zImage. For some reason, there is presence of 0xaa in the first word and it causing issue. The Mfgtool is &lt;U&gt;not&lt;/U&gt; able to go beyond the Bootstrap phase.&lt;/P&gt;&lt;P&gt;Did anybody come across the issue? How can this be resolved?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 08:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-2-0-UTP-corrupting-image-data-while-loading-during/m-p/1135051#M161058</guid>
      <dc:creator>arindamroy</dc:creator>
      <dc:date>2020-09-03T08:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool 2.0 (UTP) corrupting image data while loading during bootstrap mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-2-0-UTP-corrupting-image-data-while-loading-during/m-p/1135169#M161074</link>
      <description>&lt;P&gt;Hi&amp;nbsp;arindamroy&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;mfgtool is supposed to enable loading of zImage, DTB and rootfs after u-boot.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;this is true only for NXP reference boards, custom board can hang.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;First, run ddr test and update Mfg Tool firmware &lt;BR /&gt;image with new ddr calibration coefficients found from test &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/1108221" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/1108221&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Update coefficients in dcd header, for example for&amp;nbsp; i.MX6Q:&amp;nbsp; uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg and&lt;BR /&gt;rebuild Mfg Tool firmware (files in ../firmware folder, &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot).&lt;BR /&gt;For rebuilding please use sect.6.2 Manufacturing Tool, MFGTool Yocto Guide&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;included in&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS" target="_blank"&gt;Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;.Use NXP Linux repository:&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Below example mfg tool with custom board&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://developer.rigado.com/docsets/Working-with-the-Rigado-Vesta-Gateway/latest/production/deploying-image-mfgtool.html" target="_blank"&gt;https://developer.rigado.com/docsets/Working-with-the-Rigado-Vesta-Gateway/latest/production/deploying-image-mfgtool.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;BR /&gt;igor&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 10:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-2-0-UTP-corrupting-image-data-while-loading-during/m-p/1135169#M161074</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-03T10:46:59Z</dc:date>
    </item>
  </channel>
</rss>