<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6D MIPI application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1134963#M161047</link>
    <description>&lt;P&gt;yes such approach is feasible.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Thu, 03 Sep 2020 06:57:36 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-09-03T06:57:36Z</dc:date>
    <item>
      <title>I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133139#M160939</link>
      <description>&lt;P&gt;1、We now use two I.M X6D CPU, one used for liquid crystal instrument, one for in-car entertainment systems, we now need for video transmission between two products, such as the need to map the IVI map synchronization to the above, we plan to the IVI of MIPI DSI interface connected to the instrument of MIPI CSI, whether to support direct connection, good software do? Is the software currently supported? If workload changes are not supported? This connection mode supports what is maximum transfer？&lt;/P&gt;&lt;P&gt;2、&lt;SPAN&gt;What is the largest version of Android currently supported on the official website? If you want to do a higher version of how to carry out？&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 14:37:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133139#M160939</guid>
      <dc:creator>tommyduan</dc:creator>
      <dc:date>2020-09-01T14:37:52Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133413#M160950</link>
      <description>&lt;P&gt;Hi tommyduan&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. for MIPI DSI / MIPI CSI software one can look at&lt;/P&gt;
&lt;P&gt;sect.6.1.4 MIPI Camera Serial Interface, sect.6.4.2 MIPI DSI Interface&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank"&gt;i.MX Linux Reference Manual​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;all linux documentation&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2. one can look at android documentation&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 00:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133413#M160950</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-02T00:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133700#M160972</link>
      <description>&lt;P&gt;1、Is the approach I describe chip supported? Is it feasible? Does the existing software meet the requirements?&lt;/P&gt;&lt;P&gt;2、Android release notes, let's take a look at the IMX8 series and see if there is i.X6 related？&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 05:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1133700#M160972</guid>
      <dc:creator>tommyduan</dc:creator>
      <dc:date>2020-09-02T05:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1134936#M161041</link>
      <description>Is the current hardware solution feasible?</description>
      <pubDate>Thu, 03 Sep 2020 06:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1134936#M161041</guid>
      <dc:creator>tommyduan</dc:creator>
      <dc:date>2020-09-03T06:31:31Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1134963#M161047</link>
      <description>&lt;P&gt;yes such approach is feasible.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 06:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1134963#M161047</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-03T06:57:36Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6D MIPI application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1149252#M161278</link>
      <description>Mipi DSI interface, the chip only supports 2 lines, what is the maximum resolution it can output? MIPI DSI directly connected to CSI Protocol support? Current software support?</description>
      <pubDate>Sat, 05 Sep 2020 14:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6D-MIPI-application/m-p/1149252#M161278</guid>
      <dc:creator>tommyduan</dc:creator>
      <dc:date>2020-09-05T14:18:03Z</dc:date>
    </item>
  </channel>
</rss>