<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB device not detected</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-device-not-detected/m-p/1134333#M161008</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am designing a custom board with an i.MX6ULL processor with&amp;nbsp;Linux version 4.14.78.&lt;/P&gt;&lt;P&gt;The uuu tool succeed in programming the eMMC with the&amp;nbsp;fsl-image-qt5-validation-imx-imx6ull14x14evk.sdcard.bz2 file by using the USB port. When the board is ready (u-boot loaded and command prompt available on serial link), I plug a USB key but nothing appears (dmesg don't show any change). On previous prototype cards with same hardware the USB key was detected.&lt;/P&gt;&lt;P&gt;With memtool utility I have the following values on the registers PMU_REG_3P00 and&amp;nbsp;PMU_MISC10:&lt;/P&gt;&lt;P&gt;root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8120 1&lt;BR /&gt;E&lt;BR /&gt;Reading 0x1 count starting at address 0x020C8120&lt;/P&gt;&lt;P&gt;0x020C8120: 00011775&lt;/P&gt;&lt;P&gt;root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8160 1&lt;BR /&gt;E&lt;BR /&gt;Reading 0x1 count starting at address 0x020C8160&lt;/P&gt;&lt;P&gt;0x020C8160: 00030000&lt;/P&gt;&lt;P&gt;This values are the same on the working and not working boards. The voltage on VDD_USB_CAP pin is 3.2V as expected. The USB key is supplied with an external +5V regulator.&lt;/P&gt;&lt;P&gt;My question is why USB key is not detected whereas uuu has successfully programmed the eMMC over USB port?&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;VP&lt;/P&gt;</description>
    <pubDate>Wed, 02 Sep 2020 14:26:07 GMT</pubDate>
    <dc:creator>vincent_pelissi</dc:creator>
    <dc:date>2020-09-02T14:26:07Z</dc:date>
    <item>
      <title>USB device not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-device-not-detected/m-p/1134333#M161008</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am designing a custom board with an i.MX6ULL processor with&amp;nbsp;Linux version 4.14.78.&lt;/P&gt;&lt;P&gt;The uuu tool succeed in programming the eMMC with the&amp;nbsp;fsl-image-qt5-validation-imx-imx6ull14x14evk.sdcard.bz2 file by using the USB port. When the board is ready (u-boot loaded and command prompt available on serial link), I plug a USB key but nothing appears (dmesg don't show any change). On previous prototype cards with same hardware the USB key was detected.&lt;/P&gt;&lt;P&gt;With memtool utility I have the following values on the registers PMU_REG_3P00 and&amp;nbsp;PMU_MISC10:&lt;/P&gt;&lt;P&gt;root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8120 1&lt;BR /&gt;E&lt;BR /&gt;Reading 0x1 count starting at address 0x020C8120&lt;/P&gt;&lt;P&gt;0x020C8120: 00011775&lt;/P&gt;&lt;P&gt;root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8160 1&lt;BR /&gt;E&lt;BR /&gt;Reading 0x1 count starting at address 0x020C8160&lt;/P&gt;&lt;P&gt;0x020C8160: 00030000&lt;/P&gt;&lt;P&gt;This values are the same on the working and not working boards. The voltage on VDD_USB_CAP pin is 3.2V as expected. The USB key is supplied with an external +5V regulator.&lt;/P&gt;&lt;P&gt;My question is why USB key is not detected whereas uuu has successfully programmed the eMMC over USB port?&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;VP&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 14:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-device-not-detected/m-p/1134333#M161008</guid>
      <dc:creator>vincent_pelissi</dc:creator>
      <dc:date>2020-09-02T14:26:07Z</dc:date>
    </item>
    <item>
      <title>Re: USB device not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-device-not-detected/m-p/1134720#M161020</link>
      <description>&lt;P&gt;Hi vincent_pelissi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for usb stick please check that USB_ID signal is low, for uuu tool&lt;/P&gt;
&lt;P&gt;i.MX is working as usb device and this signal is high or floating.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 23:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-device-not-detected/m-p/1134720#M161020</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-02T23:46:59Z</dc:date>
    </item>
  </channel>
</rss>