<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error in yocto build while creating image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1133097#M160926</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello Nishitha,&lt;/P&gt;
&lt;P&gt;It looks like debian issue but Which release of the project is this? Are you using any buildtools&lt;BR /&gt;tarball? Is uninative enabled?&lt;/P&gt;
&lt;P&gt;It sounds like there is missing codepage/locale data. Whether that is&lt;BR /&gt;on the host system or from the project, its hard to say based on the&lt;BR /&gt;limited info about the version/configuration.&lt;/P&gt;
&lt;P&gt;Try to use ubuntu 18.04, it will work.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 01 Sep 2020 13:41:47 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-09-01T13:41:47Z</dc:date>
    <item>
      <title>Error in yocto build while creating image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1076933#M158081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am doing yocto build for imx8m board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The bitbake is 99% complete and then I get this error. Please provide suggestions to remove the issue.&lt;/P&gt;&lt;P&gt;Host is debian 8.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake imx-image-multimedia&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.44.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "debian-8"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "imx8mqevk"&lt;BR /&gt;DISTRO = "fsl-imx-wayland"&lt;BR /&gt;DISTRO_VERSION = "5.4-zeus"&lt;BR /&gt;TUNE_FEATURES = "aarch64 cortexa53 crc crypto"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:cba967414370e195d109353e51510bd829aa86c3"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia &lt;BR /&gt;meta-python = "HEAD:9e60d30669a2ad0598e9abf0cd15ee06b523986b"&lt;BR /&gt;meta-freescale = "HEAD:c2a0d924f6200eea1fb1d1b61e7420ea5da2f8fb"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:dbcc686f52c3c84db8cb86aa8973a4e373651b98"&lt;BR /&gt;meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk &lt;BR /&gt;meta-ml = "HEAD:a083ffbbc3f4d1c02b1542746784d7f641a75b60"&lt;BR /&gt;meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"&lt;BR /&gt;meta-rust = "HEAD:a012a1027defe28495f06ed522a7a82bdd59a610"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-filesystems = "HEAD:9e60d30669a2ad0598e9abf0cd15ee06b523986b"&lt;BR /&gt;meta-qt5 = "HEAD:b8bcf8cb576d072f435a0177375e54424f67d1c9"&lt;BR /&gt;meta-python2 = "HEAD:231c3d74cfcf734c3415e86ea8dd97f73ddced9d"&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Execution of '/home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/temp/run.do_image_wic.29521' failed with exit code 1:&lt;BR /&gt;| INFO: Creating image(s)...&lt;BR /&gt;| &lt;BR /&gt;| ERROR: _exec_cmd: export PATH=/home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/recipe-sysroot-native/sbin:/home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/recipe-sysroot-native/usr/sbin:/home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/recipe-sysroot-native/usr/bin:$PATH;mcopy -i /home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/deploy-imx-image-multimedia-image-complete/imx-image-multimedia-imx8mqevk-20200828095555/tmp.wic.d_b7c976/rootfs_boot.2.vfat -s /home/nishitha/imx-yocto-bsp/build_imx/tmp/work/imx8mqevk-poky-linux/imx-image-multimedia/1.0-r0/deploy-imx-image-multimedia-image-complete/imx-image-multimedia-imx8mqevk-20200828095555/tmp.wic.d_b7c976/boot.2/* ::/ returned '1' instead of 0&lt;BR /&gt;| output: Error converting to codepage 850 Invalid argument&lt;BR /&gt;| Cannot initialize '::'&lt;BR /&gt;| Bad target ::/&lt;BR /&gt;| &lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| &lt;BR /&gt;ERROR: Task (/home/nishitha/imx-yocto-bsp/sources/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_image_wic) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 6918 tasks of which 6917 didn't need to be rerun and 1 failed.&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 10:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1076933#M158081</guid>
      <dc:creator>nishitha_a</dc:creator>
      <dc:date>2020-08-28T10:22:12Z</dc:date>
    </item>
    <item>
      <title>Error in yocto build while creating image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1133097#M160926</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello Nishitha,&lt;/P&gt;
&lt;P&gt;It looks like debian issue but Which release of the project is this? Are you using any buildtools&lt;BR /&gt;tarball? Is uninative enabled?&lt;/P&gt;
&lt;P&gt;It sounds like there is missing codepage/locale data. Whether that is&lt;BR /&gt;on the host system or from the project, its hard to say based on the&lt;BR /&gt;limited info about the version/configuration.&lt;/P&gt;
&lt;P&gt;Try to use ubuntu 18.04, it will work.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 13:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1133097#M160926</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-09-01T13:41:47Z</dc:date>
    </item>
    <item>
      <title>Re: Error in yocto build while creating image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1149456#M161302</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;I have tried the same in Ubuntu 18.04 and gets stuck at the same issue there also.&lt;/P&gt;&lt;P&gt;I do use&amp;nbsp;&lt;SPAN&gt;prebuilt “buildtools tarballs" for installing the dependencies. The installation is done as below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;I&gt;sh x86_64-buildtools-nativesdk-standalone-3.1.sh&lt;/I&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;I&gt;sh x86_64-buildtools-extended-nativesdk-standalone-3.1.sh&lt;/I&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I follow the steps from the latest 2020 document&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These are the steps done :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&lt;SPAN&gt;source /opt/poky/3.1/environment-setup-x86_64-pokysdk-linux&lt;/SPAN&gt;&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;I&gt;cd imx-yocto-bsp&lt;/I&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;I&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml&lt;/I&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;I&gt;repo sync&lt;/I&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;I&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build_imx&lt;/I&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;I&gt;bitbake imx-image-multimedia&lt;/I&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 06:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1149456#M161302</guid>
      <dc:creator>nishitha_a</dc:creator>
      <dc:date>2020-09-07T06:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: Error in yocto build while creating image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1150093#M161399</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;I had tried in Ubuntu 18.04 also, but there also I get the same issue.&lt;/P&gt;&lt;P&gt;I follow the latest 2020 document&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I am using prebuilt tarballs from&amp;nbsp;&lt;A href="http://downloads.yoctoproject.org/releases/yocto/yocto-3.1/buildtools/" target="_blank" rel="noopener"&gt;http://downloads.yoctoproject.org/releases/yocto/yocto-3.1/buildtools/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;These are the steps followed in detail :&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Source tools environment&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;&lt;I&gt;&lt;SPAN&gt;source /opt/poky/3.1/environment-setup-x86_64-pokysdk-linux&lt;/SPAN&gt;&lt;/I&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;I&gt;&lt;SPAN&gt;Repo init &lt;/SPAN&gt;&lt;/I&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;&amp;nbsp;mkdir imx-yocto-bsp&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;&amp;nbsp;cd imx-yocto-bsp&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;repo init -u &lt;/SPAN&gt;&lt;/I&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank" rel="noopener"&gt;&lt;I&gt;&lt;SPAN&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/SPAN&gt;&lt;/I&gt;&lt;/A&gt;&lt;I&gt;&lt;SPAN&gt; -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;repo sync&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;I&gt;&lt;SPAN&gt;Build&lt;/SPAN&gt;&lt;/I&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build_imx&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;bitbake imx-image-multimedia&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 06:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1150093#M161399</guid>
      <dc:creator>nishitha_a</dc:creator>
      <dc:date>2020-09-08T06:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: Error in yocto build while creating image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1150097#M161400</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;I had tried in Ubuntu 18.04 also, but there also I get the same issue.&lt;/P&gt;&lt;P&gt;I follow the latest 2020 document&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank" rel="noopener nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I am using prebuilt tarballs from&amp;nbsp;&lt;A href="http://downloads.yoctoproject.org/releases/yocto/yocto-3.1/buildtools/" target="_blank" rel="noopener nofollow noopener noreferrer"&gt;http://downloads.yoctoproject.org/releases/yocto/yocto-3.1/buildtools/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;These are the steps followed in detail :&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Source tools environment&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;&lt;I&gt;&lt;SPAN&gt;source /opt/poky/3.1/environment-setup-x86_64-pokysdk-linux&lt;/SPAN&gt;&lt;/I&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;I&gt;&lt;SPAN&gt;Repo init&lt;/SPAN&gt;&lt;/I&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;&amp;nbsp;mkdir imx-yocto-bsp&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;&amp;nbsp;cd imx-yocto-bsp&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;repo init -u&amp;nbsp;&lt;/SPAN&gt;&lt;/I&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank" rel="noopener nofollow noopener noreferrer"&gt;&lt;I&gt;&lt;SPAN&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/SPAN&gt;&lt;/I&gt;&lt;/A&gt;&lt;I&gt;&lt;SPAN&gt;&amp;nbsp;-b imx-linux-zeus -m imx-5.4.24-2.1.0.xml&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;repo sync&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;I&gt;&lt;SPAN&gt;Build&lt;/SPAN&gt;&lt;/I&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build_imx&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;I&gt;&lt;SPAN&gt;bitbake imx-image-multimedia&lt;/SPAN&gt;&lt;/I&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 08 Sep 2020 06:42:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-yocto-build-while-creating-image/m-p/1150097#M161400</guid>
      <dc:creator>nishitha_a</dc:creator>
      <dc:date>2020-09-08T06:42:37Z</dc:date>
    </item>
  </channel>
</rss>