<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6ULL evaluation board NAND support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132785#M160880</link>
    <description>&lt;P&gt;In the imX6ULL evaluation board schematic on the page for Flash there is a&amp;nbsp;MTFC8GACAAAM on the lower left. It is not connected to anything as far as I can see. Am I right? I think it is just a footprint. Why is it there? I want to solder a BGA NAND flash to the board but this footprint seems to be not connected electrically to anything. i want to see whether I have missed anything. Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Sep 2020 01:27:23 GMT</pubDate>
    <dc:creator>awong121</dc:creator>
    <dc:date>2020-09-01T01:27:23Z</dc:date>
    <item>
      <title>iMX6ULL evaluation board NAND support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132785#M160880</link>
      <description>&lt;P&gt;In the imX6ULL evaluation board schematic on the page for Flash there is a&amp;nbsp;MTFC8GACAAAM on the lower left. It is not connected to anything as far as I can see. Am I right? I think it is just a footprint. Why is it there? I want to solder a BGA NAND flash to the board but this footprint seems to be not connected electrically to anything. i want to see whether I have missed anything. Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 01:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132785#M160880</guid>
      <dc:creator>awong121</dc:creator>
      <dc:date>2020-09-01T01:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL evaluation board NAND support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132801#M160882</link>
      <description>&lt;P&gt;It's for TSOP-48 NAND.&amp;nbsp;&lt;A href="http://nxp.com/doc/imx6ullevkhug" target="_blank"&gt;http://nxp.com/doc/imx6ullevkhug&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 02:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132801#M160882</guid>
      <dc:creator>mike_nxp_commun</dc:creator>
      <dc:date>2020-09-01T02:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL evaluation board NAND support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132815#M160885</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/124916"&gt;@awong121&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; MTFC8GACAAAM is eMMC. According to section 2.6 (eMMC)of i.MX 6ULL EVK Board Hardware User's Guide:&lt;BR /&gt;The eMMC interface is connected to USDHC2 of i.MX 6ULL. It can support up to eMMC 4.5, the&lt;BR /&gt;eMMC device is not populated by default on the EVK board. To boot from eMMC, remove the Micro SD&lt;BR /&gt;socket and populate the eMMC device, and then change the boot device switch (SW601) settings&lt;BR /&gt;(OFF, ON, ON, OFF) as shown in Table 3 Additionally, the BOOT_CFG settings must be adjusted for&lt;BR /&gt;the specified eMMC device by exchanging the pull up/down resistors.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;A href="http://nxp.com/doc/imx6ullevkhug" target="_blank" rel="noopener"&gt;http://nxp.com/doc/imx6ullevkhug&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NAND on the EVK is mentioned as MT29F32G08CBADBW. Use section 2.8 (NAND flash) of the Guide&lt;BR /&gt;for more details.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 03:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-evaluation-board-NAND-support/m-p/1132815#M160885</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-09-01T03:12:41Z</dc:date>
    </item>
  </channel>
</rss>