<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6ull spi slave mode txfifo error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-slave-mode-txfifo-error/m-p/1095249#M160439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used imx6ull's ECSPI3 SS_0 channel and configured it in slave mode at a rate of 20Mhz;&lt;BR /&gt;The BURST_LENGTH of ECSPI3 is set to 1599, that is, 50 words are transferred at a time, and the software will write 50 words to TXDATA continuously in each transfer.&lt;BR /&gt;Master uses Linux 3.4.2, Master and slave's CPOL=CPHA=0.&lt;BR /&gt;Part of the data received by the master in the experiment is shown in the following figure. Basically, garbled codes will be generated for every 50 data received.&lt;BR /&gt;However, when I add 1ms delay to the loop of the master receiving data, the received data will be normal.&lt;BR /&gt;I don't know what the reason is, is it because txdata's fifo needs 1ms to clear after it is full?&lt;BR /&gt;Hope someone can answer my questions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="InkedQQ图片20200518113236_LI.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107381iF1991BC9C11BC858/image-size/large?v=v2&amp;amp;px=999" role="button" title="InkedQQ图片20200518113236_LI.jpg" alt="InkedQQ图片20200518113236_LI.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2020 03:45:52 GMT</pubDate>
    <dc:creator>1486662470</dc:creator>
    <dc:date>2020-05-18T03:45:52Z</dc:date>
    <item>
      <title>imx6ull spi slave mode txfifo error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-slave-mode-txfifo-error/m-p/1095249#M160439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used imx6ull's ECSPI3 SS_0 channel and configured it in slave mode at a rate of 20Mhz;&lt;BR /&gt;The BURST_LENGTH of ECSPI3 is set to 1599, that is, 50 words are transferred at a time, and the software will write 50 words to TXDATA continuously in each transfer.&lt;BR /&gt;Master uses Linux 3.4.2, Master and slave's CPOL=CPHA=0.&lt;BR /&gt;Part of the data received by the master in the experiment is shown in the following figure. Basically, garbled codes will be generated for every 50 data received.&lt;BR /&gt;However, when I add 1ms delay to the loop of the master receiving data, the received data will be normal.&lt;BR /&gt;I don't know what the reason is, is it because txdata's fifo needs 1ms to clear after it is full?&lt;BR /&gt;Hope someone can answer my questions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="InkedQQ图片20200518113236_LI.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107381iF1991BC9C11BC858/image-size/large?v=v2&amp;amp;px=999" role="button" title="InkedQQ图片20200518113236_LI.jpg" alt="InkedQQ图片20200518113236_LI.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 03:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-slave-mode-txfifo-error/m-p/1095249#M160439</guid>
      <dc:creator>1486662470</dc:creator>
      <dc:date>2020-05-18T03:45:52Z</dc:date>
    </item>
  </channel>
</rss>