<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux system clock when iMX6 is in deepsleep in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094550#M160370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX6 processor with Linux OS in a project. Can you please let me know whether linux system clock will be running when the iMX6 is in deepsleep mode? If it will not be running, how the system clock will be updated in when the iMX6 wakes up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sivaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2020 17:20:37 GMT</pubDate>
    <dc:creator>sivaraj</dc:creator>
    <dc:date>2020-05-15T17:20:37Z</dc:date>
    <item>
      <title>Linux system clock when iMX6 is in deepsleep</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094550#M160370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX6 processor with Linux OS in a project. Can you please let me know whether linux system clock will be running when the iMX6 is in deepsleep mode? If it will not be running, how the system clock will be updated in when the iMX6 wakes up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sivaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 17:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094550#M160370</guid>
      <dc:creator>sivaraj</dc:creator>
      <dc:date>2020-05-15T17:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: Linux system clock when iMX6 is in deepsleep</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094551#M160371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sivaraj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Deep sleep mode is implemented in linux, please check&amp;nbsp; &lt;BR /&gt;Chapter 21 Low-level Power Management (PM) Driver of the&amp;nbsp; Linux Manual for description of Mem (suspend to RAM) mode and AN4509 i.MX 6Dual/6Quad Power Consumption Measurement sect. Deep Sleep Mode&lt;BR /&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4509.pdf" rel="nofollow" target="_blank"&gt;https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf&lt;/A&gt;&lt;BR /&gt;Note, if custom modifications of linux sources are needed, may be recommended&lt;BR /&gt;to apply to profesional services or elevate request through local fae channel (project info&lt;BR /&gt;may be needed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 13:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094551#M160371</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-05-18T13:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: Linux system clock when iMX6 is in deepsleep</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094552#M160372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I am trying to understand how the linux system clock works in the deepsleep mode of iMX6 processor. I could not get the answer from the documents.&lt;/P&gt;&lt;P&gt;Can you please help me understand?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 06:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-system-clock-when-iMX6-is-in-deepsleep/m-p/1094552#M160372</guid>
      <dc:creator>sivaraj</dc:creator>
      <dc:date>2020-05-19T06:38:29Z</dc:date>
    </item>
  </channel>
</rss>