<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic In Serial Downloader mode, download using USB, PC does not link to USB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/In-Serial-Downloader-mode-download-using-USB-PC-does-not-link-to/m-p/1094218#M160324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my design, i.mx6ul's UART2_RXD, UART4_RXD, UART5_RXD connected to other MCUs of UART.Internal Boot start-up, i.mx6ul and MCU's UART data communication is no problem.&lt;BR /&gt;When in Serial Downloader mode, and this MCU is working, using USB download, the PC does not link to USB.&lt;BR /&gt;If the MCU stops working, the PC can link to USB and download it complete.&lt;BR /&gt;Is there a BUG in i.mx6ul?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2020 08:48:28 GMT</pubDate>
    <dc:creator>353533661</dc:creator>
    <dc:date>2020-04-29T08:48:28Z</dc:date>
    <item>
      <title>In Serial Downloader mode, download using USB, PC does not link to USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/In-Serial-Downloader-mode-download-using-USB-PC-does-not-link-to/m-p/1094218#M160324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my design, i.mx6ul's UART2_RXD, UART4_RXD, UART5_RXD connected to other MCUs of UART.Internal Boot start-up, i.mx6ul and MCU's UART data communication is no problem.&lt;BR /&gt;When in Serial Downloader mode, and this MCU is working, using USB download, the PC does not link to USB.&lt;BR /&gt;If the MCU stops working, the PC can link to USB and download it complete.&lt;BR /&gt;Is there a BUG in i.mx6ul?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 08:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/In-Serial-Downloader-mode-download-using-USB-PC-does-not-link-to/m-p/1094218#M160324</guid>
      <dc:creator>353533661</dc:creator>
      <dc:date>2020-04-29T08:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: In Serial Downloader mode, download using USB, PC does not link to USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/In-Serial-Downloader-mode-download-using-USB-PC-does-not-link-to/m-p/1094219#M160325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xiaojun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to Figure 8-2. Serial Downloader boot flow&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6ULRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6UltraLite Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;both uart and usb are polling by ROM. So uart activity may prevent&lt;/P&gt;&lt;P&gt;PC link to USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 10:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/In-Serial-Downloader-mode-download-using-USB-PC-does-not-link-to/m-p/1094219#M160325</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-04-29T10:17:29Z</dc:date>
    </item>
  </channel>
</rss>