<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Does NXP provide any stable and bugfix updates to BSP kernel?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-provide-any-stable-and-bugfix-updates-to-BSP-kernel/m-p/1093714#M160240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest BSP update is the L5.4.3 and you can download from the code aurora as well. there is no any update from the L4.19.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jun 2020 17:10:12 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-06-29T17:10:12Z</dc:date>
    <item>
      <title>Does NXP provide any stable and bugfix updates to BSP kernel?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-provide-any-stable-and-bugfix-updates-to-BSP-kernel/m-p/1093713#M160239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using i.MX 8M Mini with a v4.19 kernel from&amp;nbsp;NXP/Codeaurora (imx_4.19.35_1.1.0). It's a pretty old release (v4.19.35) from v4.19 stable tree with a lot of unfixed bugs. The current v4.19 kernel is v4.19.130, so almost 100 stable releases further.&lt;/P&gt;&lt;P&gt;These stable releases come with a lot less and more important bug fixes (including security fixes).&lt;/P&gt;&lt;P&gt;The question: Do you plan to provide BSP v4.19 kernel updated to latest stable v4.19 (e.g. v4.19.130) or you expect every customer should perform such &lt;STRONG&gt;important&amp;nbsp;maintenance by himself&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Krzysztof&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 11:21:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-provide-any-stable-and-bugfix-updates-to-BSP-kernel/m-p/1093713#M160239</guid>
      <dc:creator>krzysztof_kozlo</dc:creator>
      <dc:date>2020-06-26T11:21:17Z</dc:date>
    </item>
    <item>
      <title>Re: Does NXP provide any stable and bugfix updates to BSP kernel?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-provide-any-stable-and-bugfix-updates-to-BSP-kernel/m-p/1093714#M160240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest BSP update is the L5.4.3 and you can download from the code aurora as well. there is no any update from the L4.19.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 17:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-provide-any-stable-and-bugfix-updates-to-BSP-kernel/m-p/1093714#M160240</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-06-29T17:10:12Z</dc:date>
    </item>
  </channel>
</rss>