<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Local Alpha Blending in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Local-Alpha-Blending/m-p/225843#M16019</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our setup&amp;nbsp; is like data from android surface flinger is available "/dev/graphics/fb0"&lt;/P&gt;&lt;P&gt;We want to do overlay with CSI buffer which is written on "/dev/graphics/fb1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are able to get it working with global alpha and colour keying. But due to some limitation with our GUI we can not use global alpha.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But If I disable global alpha and enable the local alpha than data from /dev/graphics/fb1 is not display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is it possible to do alpha blending using local alpha without colour keying?&lt;/P&gt;&lt;P&gt;- What is a significance of alpha_phy_addr0, alpha_phy_addr1 and alpha_in_pixel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jul 2013 14:03:52 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2013-07-26T14:03:52Z</dc:date>
    <item>
      <title>Local Alpha Blending</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Local-Alpha-Blending/m-p/225843#M16019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our setup&amp;nbsp; is like data from android surface flinger is available "/dev/graphics/fb0"&lt;/P&gt;&lt;P&gt;We want to do overlay with CSI buffer which is written on "/dev/graphics/fb1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are able to get it working with global alpha and colour keying. But due to some limitation with our GUI we can not use global alpha.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But If I disable global alpha and enable the local alpha than data from /dev/graphics/fb1 is not display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is it possible to do alpha blending using local alpha without colour keying?&lt;/P&gt;&lt;P&gt;- What is a significance of alpha_phy_addr0, alpha_phy_addr1 and alpha_in_pixel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2013 14:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Local-Alpha-Blending/m-p/225843#M16019</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2013-07-26T14:03:52Z</dc:date>
    </item>
  </channel>
</rss>