<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 More UART connectivity</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093333#M160166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,iMX6ULZ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently running Linux on iMX6ULZ SoC 4 x UART but I need one or two more UART, which iMX6 or iMX7 SoC I can select? I can use the NXP MFGTools to flash image to iMX6ULZ NAND, will the same tools compatible for all other iMX6 or iMX7 SoC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jhiMX6ULZ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2020 10:04:59 GMT</pubDate>
    <dc:creator>jupiter_hce</dc:creator>
    <dc:date>2020-06-26T10:04:59Z</dc:date>
    <item>
      <title>More UART connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093333#M160166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,iMX6ULZ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently running Linux on iMX6ULZ SoC 4 x UART but I need one or two more UART, which iMX6 or iMX7 SoC I can select? I can use the NXP MFGTools to flash image to iMX6ULZ NAND, will the same tools compatible for all other iMX6 or iMX7 SoC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jhiMX6ULZ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 10:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093333#M160166</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2020-06-26T10:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: More UART connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093334#M160167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jupiter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at i.MX6 comparison table&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf" title="https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf"&gt;https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 11:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093334#M160167</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-26T11:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: More UART connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093335#M160168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response and the link, but there are more discrepancies between the two documents, in the document&amp;nbsp; i.MX 6ULZ Applications Processors that the number of UART is 4 which I think is correct, where the &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fbrochure%2FFLYRIMXPRDCMPR.pdf" rel="nofollow" target="_blank"&gt;FLYRIMXPRDCMPR.pdf&lt;/A&gt; that the number of UART is 8 which I think is wrong, could you please further clarify it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fbrochure%2FFLYRIMXPRDCMPR.pdf" rel="nofollow" target="_blank"&gt;FLYRIMXPRDCMPR.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jun 2020 01:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093335#M160168</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2020-06-28T01:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: More UART connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093336#M160169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jupiter&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;you are right, correct number of UART is 4 .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jun 2020 13:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-UART-connectivity/m-p/1093336#M160169</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-28T13:00:02Z</dc:date>
    </item>
  </channel>
</rss>