<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックNew i.MX51 System On Module -blog archive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/New-i-MX51-System-On-Module-blog-archive/m-p/153204#M1600</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ARMadeus Systems is proud to announce its new i.MX51 based SOM: the APF51.&lt;/P&gt;&lt;P&gt;It is based on an i.MX515 @ 800MHz with 64 to 512MBytes of 32 bits LPDDR RAM, 256 MB to 32 GB of 8 bits SLC NAND FLASH, a Xilinx Spartan 6A FPGA and a Wolfson WM8311 PMIC.&lt;/P&gt;&lt;P&gt;More informations are available &lt;A href="http://www.armadeus.com/english/products-processor_boards-apf51.html" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;For quick development purposes, the APF51 SOM can be plugged on the APF51Dev docking board which adds it the following functionalities: WiFi b/g, Bluetooth 2.0, 8x12bits ADC, 2x10 bits DAC, CAN Bus, HDMI video output, 2x USB High Speed Host connectors, 1x USB OTG connector, Ethernet 10/100 connector, 24 bits LCD Interface, Stereo Audio In/Out, microSD connector, camera connector, FPGA IOs connector and optionally: 2G/3G Modem, GPS and Industrial Buses with HMS AnyBus (TM).&lt;/P&gt;&lt;P&gt;More informations are available &lt;A href="http://www.armadeus.com/english/products-development_boards-apf51_dev.html" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Boards are delivered with a fully functionnal BSP based on U-Boot 2010.03, Linux 2.6.38.1 and Buildroot 2010.11.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 May 2011 12:04:34 GMT</pubDate>
    <dc:creator>JulienBoibessot</dc:creator>
    <dc:date>2011-05-04T12:04:34Z</dc:date>
    <item>
      <title>New i.MX51 System On Module -blog archive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/New-i-MX51-System-On-Module-blog-archive/m-p/153204#M1600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ARMadeus Systems is proud to announce its new i.MX51 based SOM: the APF51.&lt;/P&gt;&lt;P&gt;It is based on an i.MX515 @ 800MHz with 64 to 512MBytes of 32 bits LPDDR RAM, 256 MB to 32 GB of 8 bits SLC NAND FLASH, a Xilinx Spartan 6A FPGA and a Wolfson WM8311 PMIC.&lt;/P&gt;&lt;P&gt;More informations are available &lt;A href="http://www.armadeus.com/english/products-processor_boards-apf51.html" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;For quick development purposes, the APF51 SOM can be plugged on the APF51Dev docking board which adds it the following functionalities: WiFi b/g, Bluetooth 2.0, 8x12bits ADC, 2x10 bits DAC, CAN Bus, HDMI video output, 2x USB High Speed Host connectors, 1x USB OTG connector, Ethernet 10/100 connector, 24 bits LCD Interface, Stereo Audio In/Out, microSD connector, camera connector, FPGA IOs connector and optionally: 2G/3G Modem, GPS and Industrial Buses with HMS AnyBus (TM).&lt;/P&gt;&lt;P&gt;More informations are available &lt;A href="http://www.armadeus.com/english/products-development_boards-apf51_dev.html" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Boards are delivered with a fully functionnal BSP based on U-Boot 2010.03, Linux 2.6.38.1 and Buildroot 2010.11.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2011 12:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/New-i-MX51-System-On-Module-blog-archive/m-p/153204#M1600</guid>
      <dc:creator>JulienBoibessot</dc:creator>
      <dc:date>2011-05-04T12:04:34Z</dc:date>
    </item>
  </channel>
</rss>