<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8QXP+MAX9288</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1091922#M159985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo NXP Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have integrated GSML MAX9288 for video input for our custom i.MX8QXP board. We are using kernel version 4.19.98. Currently the driver is missing. I have not found the driver for this chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone provide me with the driver?&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Hossain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jun 2020 11:18:44 GMT</pubDate>
    <dc:creator>mdmosaddekhossa</dc:creator>
    <dc:date>2020-06-25T11:18:44Z</dc:date>
    <item>
      <title>i.MX8QXP+MAX9288</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1091922#M159985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo NXP Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have integrated GSML MAX9288 for video input for our custom i.MX8QXP board. We are using kernel version 4.19.98. Currently the driver is missing. I have not found the driver for this chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone provide me with the driver?&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Hossain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2020 11:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1091922#M159985</guid>
      <dc:creator>mdmosaddekhossa</dc:creator>
      <dc:date>2020-06-25T11:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP+MAX9288</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1091923#M159986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hossain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use as reference max9286 driver, described in sect.6.1.7 V4L2 Capture&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8/max9286.c?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8/max9286.c?h=imx_4.19.35_1.1.0"&gt;max9286.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://freescale.jiveon.com/docs/DOC-344896" title="https://freescale.jiveon.com/docs/DOC-344896"&gt;AR0144 and ov9284 drivers for I.MX8QM/QXP. | NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for debugging one can try camera unit test:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test/mx8_v4l2_cap_drm.c?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test/mx8_v4l2_cap_drm.c?h=imx_5.4.3_2.0.0"&gt;mx8_v4l2_cap_drm.c\mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2020 12:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1091923#M159986</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-25T12:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP+MAX9288</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1381911#M184012</link>
      <description>&lt;P&gt;i write driver for 9288,but when i test ,application blocked at DQBUF,is there someone can help me?&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 10:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9288/m-p/1381911#M184012</guid>
      <dc:creator>yuanke</dc:creator>
      <dc:date>2021-12-06T10:43:14Z</dc:date>
    </item>
  </channel>
</rss>