<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8M MAC to MAC Communication in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-MAC-to-MAC-Communication/m-p/1090961#M159876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sahil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think connections are correct and one can use the&lt;/P&gt;&lt;P&gt;same clock oscillator to connect to both&amp;nbsp;MAC1_TxC &amp;amp;&amp;nbsp;MAC2_TxC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2020 01:20:28 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-07-13T01:20:28Z</dc:date>
    <item>
      <title>iMX8M MAC to MAC Communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-MAC-to-MAC-Communication/m-p/1090960#M159875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on one project and want to do MAC to MAC communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Requirement: iMX8M to iMX8M communication over MAC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have done following connections in the schematic:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MAC1_TxC --&amp;gt; MAC2_RxC&lt;/P&gt;&lt;P&gt;MAC1_Tx_CTL&amp;nbsp;--&amp;gt; MAC2_Rx_CTL&lt;/P&gt;&lt;P&gt;MAC1_TxD[3:0] --&amp;gt;&amp;nbsp;MAC2_RxD[3:0]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MAC1_RxC &amp;lt;-- MAC2_TxC&lt;/P&gt;&lt;P&gt;MAC1_Rx_CTL &amp;lt;-- MAC2_Tx_CTL&lt;/P&gt;&lt;P&gt;MAC1_RxD[3:0] &amp;lt;--&amp;nbsp;MAC2_TxD[3:0]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have used&amp;nbsp;external 125MHz clock source. So my question is, where do we have to connect the external clock source??&lt;/P&gt;&lt;P&gt;Do we have to connect to both&amp;nbsp;MAC1_TxC &amp;amp;&amp;nbsp;MAC2_TxC??&lt;/P&gt;&lt;P&gt;If yes, Can we use the same clock oscillator to connect to both&amp;nbsp;MAC1_TxC &amp;amp;&amp;nbsp;MAC2_TxC??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anything else need to be taken care?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please confirm on above.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Awaiting for your quick response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sahil Nayak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jul 2020 11:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-MAC-to-MAC-Communication/m-p/1090960#M159875</guid>
      <dc:creator>sahilnayak</dc:creator>
      <dc:date>2020-07-11T11:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M MAC to MAC Communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-MAC-to-MAC-Communication/m-p/1090961#M159876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sahil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think connections are correct and one can use the&lt;/P&gt;&lt;P&gt;same clock oscillator to connect to both&amp;nbsp;MAC1_TxC &amp;amp;&amp;nbsp;MAC2_TxC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 01:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-MAC-to-MAC-Communication/m-p/1090961#M159876</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-07-13T01:20:28Z</dc:date>
    </item>
  </channel>
</rss>