<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 Android Framebuffer Config for 16bit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225745#M15977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi were you able to figure this out? I am also using android 4.2.2 build and 16-bit lcd and not getting anything on my lcd. I've tested my lcd using yocto linux so I know my init sequence for initializing the lcd is ok. My android boot params are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;enable_wait_mode=off console=ttymxc0,115200 vmalloc=400M consoleblank=0 rootdelay=3 video=mxcfb0:dev=lcd,DTECH,if=RGB666 video=mxcfb1:off video=mxcfb2:off fbmem=28M fbcon=28M androidboot.bootdev=sdhci-esdhc-imx.0 androidboot.hardware=freescale androidboot.console=ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where DTECH is the name of my lcd and i've added this to mxc_lcdif as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Jul 2014 04:29:59 GMT</pubDate>
    <dc:creator>varsmolta</dc:creator>
    <dc:date>2014-07-12T04:29:59Z</dc:date>
    <item>
      <title>i.MX6 Android Framebuffer Config for 16bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225742#M15974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use a i.MX6Q SabreSD to test the framebuffer.&lt;/P&gt;&lt;P&gt;I want to make a config that:&lt;/P&gt;&lt;P&gt;HDMI output @ 1280*720P - bpp=32bit&lt;/P&gt;&lt;P&gt;and a dummy output @ 480*800 - bpp=16bit(I only want to use the frame buffer content, to copy to outsie devices as projector ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But whatever I config via command line or board***.c, the frame buffer color depth for the dummy device(ldb or lcd) always be 32bit(RGBA?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I config it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2013 16:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225742#M15974</guid>
      <dc:creator>johnson_zhang</dc:creator>
      <dc:date>2013-11-25T16:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Android Framebuffer Config for 16bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225743#M15975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;would you show what command line you used? and what changes in the board***.c?&lt;/P&gt;&lt;P&gt;also, it is better to tell what BSP and board are you using.&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2013 06:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225743#M15975</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-11-29T06:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Android Framebuffer Config for 16bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225744#M15976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jimmy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use a SabreSD board, and try to set bpp=16 for HDMI/LCD display.&lt;/P&gt;&lt;P&gt;But seems that FB0/FB2 only use RGBA format for the UI display data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What we want is try to copy RGB565 framebuffer data as treaming out, but seems Android 4.2.2 only use RGBA(32bit) for it's display device framebuffers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me check it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 16:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225744#M15976</guid>
      <dc:creator>johnson_jl</dc:creator>
      <dc:date>2013-12-02T16:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Android Framebuffer Config for 16bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225745#M15977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi were you able to figure this out? I am also using android 4.2.2 build and 16-bit lcd and not getting anything on my lcd. I've tested my lcd using yocto linux so I know my init sequence for initializing the lcd is ok. My android boot params are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;enable_wait_mode=off console=ttymxc0,115200 vmalloc=400M consoleblank=0 rootdelay=3 video=mxcfb0:dev=lcd,DTECH,if=RGB666 video=mxcfb1:off video=mxcfb2:off fbmem=28M fbcon=28M androidboot.bootdev=sdhci-esdhc-imx.0 androidboot.hardware=freescale androidboot.console=ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where DTECH is the name of my lcd and i've added this to mxc_lcdif as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jul 2014 04:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-Framebuffer-Config-for-16bit/m-p/225745#M15977</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-07-12T04:29:59Z</dc:date>
    </item>
  </channel>
</rss>