<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: BOOT FAILURE IMX6 Custom Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088523#M159598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The voltage rails are&lt;BR /&gt;VBUS - 5.145V (PMIC supply)&lt;BR /&gt;SW1 - 1.389V&lt;BR /&gt;SW2 - 1.355V&lt;BR /&gt;SW3 - 3.340V&lt;BR /&gt;VLDO1 - 1.802V&lt;BR /&gt;VLDO2 - Unconnected&lt;BR /&gt;VLDO3 - 3.296&lt;BR /&gt;VSNVS - 3.041V&lt;BR /&gt;DDR_VREF - 0.676V&lt;/P&gt;&lt;P&gt;on power on with POR_B floating POR_B - 3.309V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried powering up the board with POR_B pulled down released after &amp;gt; 5 sec - No detection&lt;BR /&gt;Tried pulling down POR_B after 10 sec of PMIC power on (initially with POR_B floating) - no detection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;XTAL&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ABS07-32.768kHZ-9-T&lt;/STRONG&gt;&lt;BR /&gt;ESR - 70kOhm&lt;BR /&gt;Load Cap - 9pF and &lt;STRONG&gt;board cap is 9pF +/- 0.1pF&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ASDMB-24.000MHZ-XY-T&lt;/STRONG&gt;&lt;BR /&gt;Stability +/- 10ppm (not checked)&lt;BR /&gt;Output load 10kOhm&lt;BR /&gt;Load Cap - 15pF&lt;BR /&gt;&lt;STRONG&gt;Board Cap 15pF (1%)&lt;/STRONG&gt;&lt;BR /&gt;Deviation - 2.2M registor to GND for XTALI bias not externally adjustable&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q: Based on the schematic i have shared, are the board caps correct?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="color: #51626f; border: 0px;"&gt;one can check board schematic using&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DIMX6ULHDG" rel="nofollow" style="color: #3d9ce7; border: 0px; font-weight: inherit; padding: 0px calc(12px + 0.35ex) 0px 0px;" target="_blank"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;Hardware Development Guide for the i.MX 6UltraLite Applications Processor&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Done that.the only deviations are&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since BOOT_MODE[1:0] have an on chip pulldown (Page 12) are not connected externally to GND at 00&lt;BR /&gt;Kept Floating&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG1_ID - Type A connector not microusb&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG1_OC&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG_PWR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am severely hampered due to lack of oscilloscope, short of that is there anything else i can try?&lt;/P&gt;&lt;P&gt;Again, any ideas are appreciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 May 2020 23:12:45 GMT</pubDate>
    <dc:creator>summertanks</dc:creator>
    <dc:date>2020-05-30T23:12:45Z</dc:date>
    <item>
      <title>BOOT FAILURE IMX6 Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088521#M159596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;I have designed and built a custom imx6 board. Design is similar to the reference diagram. The power supply is running off a NXP PF1510. The device is driven of the USB power rail (5.0V, stable supply). USB_OTG1 is connected to USB TypeA connector.&lt;/P&gt;&lt;UL style="color: #242729; border: 0px; margin: 0px 0px 1em 30px;"&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;All the power rail voltages from PMIC on power up are good (+/- 2%).&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;RESETMCU on the PMIC is good (3.3V)&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;POR_B either connected to PMIC RESETMCU or left floating is good (3.3V)&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;SI analysis of the board done on altium doesn't indicate too much overshoot or undershoot.&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit;"&gt;XTALs are ABS07-32.768KHZ-9-T and ASDMB-24.000MHZ-XY-T&lt;/LI&gt;&lt;/UL&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;Only OTG1 being used&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot 2020-05-29 at 11.44.13.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108542iA66E780DF1672B4C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2020-05-29 at 11.44.13.png" alt="Screenshot 2020-05-29 at 11.44.13.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;Connected to USB Type A&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot 2020-05-29 at 11.45.01.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108543i6C2DE7BD28186736/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2020-05-29 at 11.45.01.png" alt="Screenshot 2020-05-29 at 11.45.01.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;BOOT MODE Selector switch, ONOFF Left floating. POR with two option - driven by PMIC / Left floating&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot 2020-05-29 at 11.46.12.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108544i245B1431722D5347/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2020-05-29 at 11.46.12.png" alt="Screenshot 2020-05-29 at 11.46.12.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;A href="https://i.stack.imgur.com/0bPEb.png" style="color: var(--blue-700); border: 0px; font-weight: inherit; text-decoration: underline;"&gt;https://i.stack.imgur.com/0bPEb.png&lt;/A&gt;XTAL connected&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot 2020-05-29 at 11.46.48.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108545iA0AAD94A27316E48/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2020-05-29 at 11.46.48.png" alt="Screenshot 2020-05-29 at 11.46.48.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;THE PROBLEM STATEMENT&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;When connected to the PC (MAC/Linux/Windows) the device is not detected (should come up as HID).&lt;/P&gt;&lt;UL style="color: #242729; border: 0px; margin: 0px 0px 1em 30px;"&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;Tried do raw packet collection using wireshark, nothing there either.&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;I do not think it is a Signal Integrity issue (impedance matching has been done, differential pair lengths checked, reference plane is good).&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;Board quality looks good too, i have multiple prototypes but dosnt work on any - likely not a quality issue.&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;Checked with different boot modes (serial connect BOOTMODE[1:0] = 01, boot from fuses BOOTMODE[1:0] = 00).&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0px 0px 0.5em;"&gt;I think either the imx6 is not booting or USB is not working - left floating POR_B is high (so that's good)and the USB differential is a straight circuit untouched and well shielded (i think).&lt;/LI&gt;&lt;LI style="border: 0px; font-weight: inherit;"&gt;Since it is not detected as HID can't use Mfgtool2 for booting, so no UART.&lt;/LI&gt;&lt;/UL&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;Despite everything cannot get the device to be detected on USB&lt;/STRONG&gt;. I would appreciated any ideas anyone can give.&lt;/P&gt;&lt;P style="color: #242729; border: 0px; margin: 0px 0px 1em;"&gt;Thank you (Do not have an oscilloscope)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 07:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088521#M159596</guid>
      <dc:creator>summertanks</dc:creator>
      <dc:date>2020-05-29T07:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT FAILURE IMX6 Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088522#M159597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harkirat&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check board schematic using&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6ULHDG" target="_blank"&gt;&lt;STRONG&gt;Hardware Development Guide for the i.MX 6UltraLite Applications Processor&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;pay attention to 24MHz clock accuracy (it may affect usb detection) and power supplies&lt;/P&gt;&lt;P&gt;ripples (&amp;lt;5%). Try with several computers. Just for test one can prolong POR up to 1 sec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 23:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088522#M159597</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-29T23:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT FAILURE IMX6 Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088523#M159598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The voltage rails are&lt;BR /&gt;VBUS - 5.145V (PMIC supply)&lt;BR /&gt;SW1 - 1.389V&lt;BR /&gt;SW2 - 1.355V&lt;BR /&gt;SW3 - 3.340V&lt;BR /&gt;VLDO1 - 1.802V&lt;BR /&gt;VLDO2 - Unconnected&lt;BR /&gt;VLDO3 - 3.296&lt;BR /&gt;VSNVS - 3.041V&lt;BR /&gt;DDR_VREF - 0.676V&lt;/P&gt;&lt;P&gt;on power on with POR_B floating POR_B - 3.309V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried powering up the board with POR_B pulled down released after &amp;gt; 5 sec - No detection&lt;BR /&gt;Tried pulling down POR_B after 10 sec of PMIC power on (initially with POR_B floating) - no detection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;XTAL&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ABS07-32.768kHZ-9-T&lt;/STRONG&gt;&lt;BR /&gt;ESR - 70kOhm&lt;BR /&gt;Load Cap - 9pF and &lt;STRONG&gt;board cap is 9pF +/- 0.1pF&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ASDMB-24.000MHZ-XY-T&lt;/STRONG&gt;&lt;BR /&gt;Stability +/- 10ppm (not checked)&lt;BR /&gt;Output load 10kOhm&lt;BR /&gt;Load Cap - 15pF&lt;BR /&gt;&lt;STRONG&gt;Board Cap 15pF (1%)&lt;/STRONG&gt;&lt;BR /&gt;Deviation - 2.2M registor to GND for XTALI bias not externally adjustable&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q: Based on the schematic i have shared, are the board caps correct?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="color: #51626f; border: 0px;"&gt;one can check board schematic using&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DIMX6ULHDG" rel="nofollow" style="color: #3d9ce7; border: 0px; font-weight: inherit; padding: 0px calc(12px + 0.35ex) 0px 0px;" target="_blank"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;Hardware Development Guide for the i.MX 6UltraLite Applications Processor&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Done that.the only deviations are&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since BOOT_MODE[1:0] have an on chip pulldown (Page 12) are not connected externally to GND at 00&lt;BR /&gt;Kept Floating&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG1_ID - Type A connector not microusb&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG1_OC&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;USB_OTG_PWR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am severely hampered due to lack of oscilloscope, short of that is there anything else i can try?&lt;/P&gt;&lt;P&gt;Again, any ideas are appreciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 May 2020 23:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FAILURE-IMX6-Custom-Board/m-p/1088523#M159598</guid>
      <dc:creator>summertanks</dc:creator>
      <dc:date>2020-05-30T23:12:45Z</dc:date>
    </item>
  </channel>
</rss>