<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx28 boot up problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-boot-up-problem/m-p/153149#M1594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;did you (or anyone) find out any more about this?&amp;nbsp; I am looking at an exact copy of the behavior you described.&lt;/P&gt;&lt;P&gt;I have wince600 source for an ARM926 hw, it compiles and the resulting eboot_ivt.sb boots and loads nk.bin from sd card.&lt;/P&gt;&lt;P&gt;On the same hardware and dev environment (WinXP), for wince700 I have done some porting according to the CE6.0-to-Compact 7 porting guides (mostly path modifications; no value changes in configs).&lt;/P&gt;&lt;P&gt;The ported source compiles (VS2008+Compact7 evk) and produces eboot_ivt and nk.bin. The new nk.bin (contains more than the previous ce600 source but anyway) can be launched with the old ce600 eboot_ivt and&amp;nbsp; with the i.MX28-EVK Compact 7 reference eboot_ivt (it stumbles on memory allocation problems but launches for a start anyway).&lt;/P&gt;&lt;P&gt;After xldr::start(), the eboot init should be executed I quess. Instead the xldr is run again, indefinitely. Any ideas of what causes this and what could fix it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Aug 2012 05:43:33 GMT</pubDate>
    <dc:creator>KariJK_ng</dc:creator>
    <dc:date>2012-08-30T05:43:33Z</dc:date>
    <item>
      <title>imx28 boot up problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-boot-up-problem/m-p/153148#M1593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on imx28 and wince. I went&amp;nbsp;through&amp;nbsp;xldr and eboot and have 2 questions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all after image(-s) creation I get eboot_ivt.sb which I loaded onto sd card and booting properly until end of xldr. After that I received "Unsupported Ins" on terminal and processor is starting all over again to boot up. Another question is how xldr is setting up nand memory to boot up from there, as there is now copying eboot image or anything to ram?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2012 12:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-boot-up-problem/m-p/153148#M1593</guid>
      <dc:creator>PawelZ</dc:creator>
      <dc:date>2012-04-11T12:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 boot up problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-boot-up-problem/m-p/153149#M1594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;did you (or anyone) find out any more about this?&amp;nbsp; I am looking at an exact copy of the behavior you described.&lt;/P&gt;&lt;P&gt;I have wince600 source for an ARM926 hw, it compiles and the resulting eboot_ivt.sb boots and loads nk.bin from sd card.&lt;/P&gt;&lt;P&gt;On the same hardware and dev environment (WinXP), for wince700 I have done some porting according to the CE6.0-to-Compact 7 porting guides (mostly path modifications; no value changes in configs).&lt;/P&gt;&lt;P&gt;The ported source compiles (VS2008+Compact7 evk) and produces eboot_ivt and nk.bin. The new nk.bin (contains more than the previous ce600 source but anyway) can be launched with the old ce600 eboot_ivt and&amp;nbsp; with the i.MX28-EVK Compact 7 reference eboot_ivt (it stumbles on memory allocation problems but launches for a start anyway).&lt;/P&gt;&lt;P&gt;After xldr::start(), the eboot init should be executed I quess. Instead the xldr is run again, indefinitely. Any ideas of what causes this and what could fix it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2012 05:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-boot-up-problem/m-p/153149#M1594</guid>
      <dc:creator>KariJK_ng</dc:creator>
      <dc:date>2012-08-30T05:43:33Z</dc:date>
    </item>
  </channel>
</rss>