<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Image data is halved with MIPI-CSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Image-data-is-halved-with-MIPI-CSI/m-p/1087281#M159361</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I made a program to receive RAW12 format data from the camera by MIPI-CSI with cortex-M4 of i.MX8Mmini.&lt;BR /&gt;However, this program has the following problems.&lt;BR /&gt;When you refer to the data set by the DMA of CSI Bridge, 1 pixel of data is obtained for every 1 pixel.&lt;BR /&gt;It's missing and only half the data is set.&lt;BR /&gt;The VGA image size of RAW12 format should be 640x480x1.5=460800, but only 230400 can be received.&lt;/P&gt;&lt;P&gt;I intend to set registers that are likely to be related to data alignment.&lt;BR /&gt;・PIXEL_BIT is 1 10-bit data for each pixel&lt;BR /&gt;・TWO_8BIT_SENSOR is 1 One 16-bit sensor is connected.&lt;/P&gt;&lt;P&gt;I'm guessing it's due to the pixel clock or byte clock.&lt;BR /&gt;Please tell me where to adjust the pixel clk and byte clock of i.MX8Mmini.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if there are other points of concern, please give us a hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;Tetsuya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2020 11:48:32 GMT</pubDate>
    <dc:creator>t-sugiyama</dc:creator>
    <dc:date>2020-06-11T11:48:32Z</dc:date>
    <item>
      <title>Image data is halved with MIPI-CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-data-is-halved-with-MIPI-CSI/m-p/1087281#M159361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I made a program to receive RAW12 format data from the camera by MIPI-CSI with cortex-M4 of i.MX8Mmini.&lt;BR /&gt;However, this program has the following problems.&lt;BR /&gt;When you refer to the data set by the DMA of CSI Bridge, 1 pixel of data is obtained for every 1 pixel.&lt;BR /&gt;It's missing and only half the data is set.&lt;BR /&gt;The VGA image size of RAW12 format should be 640x480x1.5=460800, but only 230400 can be received.&lt;/P&gt;&lt;P&gt;I intend to set registers that are likely to be related to data alignment.&lt;BR /&gt;・PIXEL_BIT is 1 10-bit data for each pixel&lt;BR /&gt;・TWO_8BIT_SENSOR is 1 One 16-bit sensor is connected.&lt;/P&gt;&lt;P&gt;I'm guessing it's due to the pixel clock or byte clock.&lt;BR /&gt;Please tell me where to adjust the pixel clk and byte clock of i.MX8Mmini.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if there are other points of concern, please give us a hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;Tetsuya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 11:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-data-is-halved-with-MIPI-CSI/m-p/1087281#M159361</guid>
      <dc:creator>t-sugiyama</dc:creator>
      <dc:date>2020-06-11T11:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: Image data is halved with MIPI-CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-data-is-halved-with-MIPI-CSI/m-p/1087282#M159362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After setting MIPI_CSI_ISP_CONFIGn and MIPI_CSI_ISP_RESOLUTIONn, when I set CSI_EN of MIPI_CSI_CSIS_COMMON_CTRL to ENABLE, I set the bit of UPDATE_SHADOW to 1 and solved it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 04:30:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-data-is-halved-with-MIPI-CSI/m-p/1087282#M159362</guid>
      <dc:creator>t-sugiyama</dc:creator>
      <dc:date>2020-06-16T04:30:21Z</dc:date>
    </item>
  </channel>
</rss>