<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SCFW and cortex-A lpuart in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087069#M159350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2020 12:26:18 GMT</pubDate>
    <dc:creator>rkohli2000</dc:creator>
    <dc:date>2020-08-13T12:26:18Z</dc:date>
    <item>
      <title>SCFW and cortex-A lpuart</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087067#M159348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using iMX8QM MEK. I would like to use the M4_0 UART (J18 debug port) from the Cortex-A cores (A53 or A72). I will need to change the SCFW to initialize power for the UART for Cortex-A. Also, not move it to the M4 partition. But, I'm not sure where this change for SCFW is required. Or if this is just a build flag change (D=2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to use the "imx-scfw-porting-kit-1.5.0" software and can someone suggest what are the changes to be made to SCFW ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What other initialization steps on the Cortex-A53 side can I use to access the UART debug port without any u-boot present in my image ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 21:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087067#M159348</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2020-08-12T21:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW and cortex-A lpuart</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087068#M159349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi rkohli2000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it is necessary to use imx-scfw-porting-kit, example with FlexCan can be found&lt;/P&gt;&lt;P&gt;on below link, in similar way one can change uart configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110265i7E629A4C74C93710/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-341481"&gt;System Controller Firmware 101 - Resource management service&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 23:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087068#M159349</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-12T23:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW and cortex-A lpuart</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087069#M159350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2020 12:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-and-cortex-A-lpuart/m-p/1087069#M159350</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2020-08-13T12:26:18Z</dc:date>
    </item>
  </channel>
</rss>