<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8M eval board and AR8031 phy issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-eval-board-and-AR8031-phy-issue/m-p/1086742#M159295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the i.MX8M evaluation target in JTAG boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the AR8031 phy is unresponsive when I try to read some registers. I keep getting 0x0000 for all registers. I have tried all the possible PHY addresses and still I can't get anything other then 0x0000 from the registers. MDC is set to 2.5MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something specific that needs to be done to enable the PHY device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2020 15:44:10 GMT</pubDate>
    <dc:creator>pnee</dc:creator>
    <dc:date>2020-06-24T15:44:10Z</dc:date>
    <item>
      <title>iMX8M eval board and AR8031 phy issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-eval-board-and-AR8031-phy-issue/m-p/1086742#M159295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the i.MX8M evaluation target in JTAG boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the AR8031 phy is unresponsive when I try to read some registers. I keep getting 0x0000 for all registers. I have tried all the possible PHY addresses and still I can't get anything other then 0x0000 from the registers. MDC is set to 2.5MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something specific that needs to be done to enable the PHY device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2020 15:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-eval-board-and-AR8031-phy-issue/m-p/1086742#M159295</guid>
      <dc:creator>pnee</dc:creator>
      <dc:date>2020-06-24T15:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M eval board and AR8031 phy issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-eval-board-and-AR8031-phy-issue/m-p/1086743#M159296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PJ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;may be useful to look at uboot codes enet initialization, in particular&lt;/P&gt;&lt;P&gt;function setup_fec() :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mq_evk/imx8mq_evk.c?h=imx_v2019.04_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mq_evk/imx8mq_evk.c?h=imx_v2019.04_5.4.3_2.0.0"&gt;imx8mq_evk.c\imx8mq_evk\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2020 23:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-eval-board-and-AR8031-phy-issue/m-p/1086743#M159296</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-24T23:22:12Z</dc:date>
    </item>
  </channel>
</rss>