<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.mx6 Deep Sleep Power Connections</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Deep-Sleep-Power-Connections/m-p/1086196#M159250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are attempting to implement deep sleep on our custom i.mx6 dual application.&amp;nbsp; Note that we are not using the PF0100.&amp;nbsp; Our question is,&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;if NVCC_RGMII and NVCC_ENET are connected to VDDHIGH_CAP, could that cause the weak linear regulator enabled via bit 18 (enable_weak_linreg) of the PMU_REG_2P5n to fail to turn on in DSM (Deep Sleep Mode) or to drop to ~0V?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2020 12:11:56 GMT</pubDate>
    <dc:creator>dmatthews</dc:creator>
    <dc:date>2020-05-28T12:11:56Z</dc:date>
    <item>
      <title>i.mx6 Deep Sleep Power Connections</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Deep-Sleep-Power-Connections/m-p/1086196#M159250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are attempting to implement deep sleep on our custom i.mx6 dual application.&amp;nbsp; Note that we are not using the PF0100.&amp;nbsp; Our question is,&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;if NVCC_RGMII and NVCC_ENET are connected to VDDHIGH_CAP, could that cause the weak linear regulator enabled via bit 18 (enable_weak_linreg) of the PMU_REG_2P5n to fail to turn on in DSM (Deep Sleep Mode) or to drop to ~0V?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 12:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Deep-Sleep-Power-Connections/m-p/1086196#M159250</guid>
      <dc:creator>dmatthews</dc:creator>
      <dc:date>2020-05-28T12:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Deep Sleep Power Connections</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Deep-Sleep-Power-Connections/m-p/1086197#M159251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="font-size: 11.0pt;"&gt;if NVCC_RGMII and NVCC_ENET are connected to VDDHIGH_CAP, could that cause the weak linear regulator enabled via &amp;gt;bit 18 (enable_weak_linreg) of the PMU_REG_2P5n to fail to turn on in DSM (Deep Sleep Mode) or to drop to ~0V?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general yes, behaviour may be unpredictable as &lt;SPAN style="font-size: 11.0pt;"&gt;VDDHIGH_CAP&lt;/SPAN&gt; usage is restricted as described below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108536i540B32EE5FF6D04E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG" target="_blank"&gt;&lt;STRONG&gt;IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors &lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 05:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Deep-Sleep-Power-Connections/m-p/1086197#M159251</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-29T05:22:07Z</dc:date>
    </item>
  </channel>
</rss>