<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWhy do I need a second Switch to receive two streams without judder?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083358#M158925</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two cameras A and B. Both cameras stream a H264 over RTP. Camera A with 40Mbps and camera B with 25Mbps. &lt;/P&gt;&lt;P&gt;When I connect the two cameras and my display to a Switch only camera A will show. Sometimes I got a picture form camera B. When I disconnect camera A I will see the stream of camera B.&lt;/P&gt;&lt;P&gt;But when I connect camera A and my display to Switch 1 and camera B to Switch 2 and connect both Switch by a patch cable I can receive both streams without any judder.&lt;/P&gt;&lt;P&gt;I did some inverstigations. I did a record with tcpdump and analyzed it with wireshark. There I can see that RTP frames of camera B are missing when I only use one Switch.&lt;/P&gt;&lt;P&gt;It is independent of the Switch. I tested several Swichtes (100Mbps and 1000Mbps).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I connect two cameras of type A or two cameras of type B to one Switch I can show their streams without any problems. It even works when the bandwith increase up to 90Mbps. I only got problems when I combine camera A with camera B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2020 11:50:11 GMT</pubDate>
    <dc:creator>MicMoba</dc:creator>
    <dc:date>2020-08-11T11:50:11Z</dc:date>
    <item>
      <title>Why do I need a second Switch to receive two streams without judder?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083358#M158925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two cameras A and B. Both cameras stream a H264 over RTP. Camera A with 40Mbps and camera B with 25Mbps. &lt;/P&gt;&lt;P&gt;When I connect the two cameras and my display to a Switch only camera A will show. Sometimes I got a picture form camera B. When I disconnect camera A I will see the stream of camera B.&lt;/P&gt;&lt;P&gt;But when I connect camera A and my display to Switch 1 and camera B to Switch 2 and connect both Switch by a patch cable I can receive both streams without any judder.&lt;/P&gt;&lt;P&gt;I did some inverstigations. I did a record with tcpdump and analyzed it with wireshark. There I can see that RTP frames of camera B are missing when I only use one Switch.&lt;/P&gt;&lt;P&gt;It is independent of the Switch. I tested several Swichtes (100Mbps and 1000Mbps).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I connect two cameras of type A or two cameras of type B to one Switch I can show their streams without any problems. It even works when the bandwith increase up to 90Mbps. I only got problems when I combine camera A with camera B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 11:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083358#M158925</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2020-08-11T11:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: Why do I need a second Switch to receive two streams without judder?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083359#M158926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/MicMoba"&gt;MicMoba&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please let me know more details about the system: block scheme, OS, (gstreamer) commands,&lt;/P&gt;&lt;P&gt;used to get the streams.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 04:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083359#M158926</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-08-12T04:45:55Z</dc:date>
    </item>
    <item>
      <title>Re: Why do I need a second Switch to receive two streams without judder?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083360#M158927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thanks for reply. I put a block scheme to the attachment. My OS is a Yocto based embedded Linux. Kernel 4.14.126.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Display:&lt;/P&gt;&lt;P&gt;IP: 192.168.0.75&lt;/P&gt;&lt;P&gt;Mask: 255.255.255.0&lt;/P&gt;&lt;P&gt;CPU: i.MX6Quad&lt;/P&gt;&lt;P&gt;Ehternet: 100Mbps&lt;/P&gt;&lt;P&gt;Resolution: 800x480px&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAM_A:&lt;/P&gt;&lt;P&gt;IP:192.168.0.120&lt;/P&gt;&lt;P&gt;Mask: 255.255.255.0&lt;/P&gt;&lt;P&gt;Streaming IP: 192.168.0.75&lt;/P&gt;&lt;P&gt;Streaming Port: 10002&lt;/P&gt;&lt;P&gt;Streaming MAC: Displays MAC&lt;/P&gt;&lt;P&gt;Codec: H264&lt;/P&gt;&lt;P&gt;Streaming mode: RTP over UDP&lt;/P&gt;&lt;P&gt;Bitrate: 40000kbps&lt;/P&gt;&lt;P&gt;Resolution: 1280x800px&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAM_B:&lt;/P&gt;&lt;P&gt;IP:192.168.0.100&lt;/P&gt;&lt;P&gt;Mask: 255.255.255.0&lt;/P&gt;&lt;P&gt;Streaming IP: 192.168.0.75&lt;/P&gt;&lt;P&gt;Streaming Port: 5002&lt;/P&gt;&lt;P&gt;Streaming MAC: Displays MAC&lt;/P&gt;&lt;P&gt;Codec: H264&lt;/P&gt;&lt;P&gt;Streaming mode: RTP over UDP&lt;/P&gt;&lt;P&gt;Bitrate: 25000kbps&lt;/P&gt;&lt;P&gt;Resolution: 1280x800px&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Switch:&lt;/P&gt;&lt;P&gt;I tried several Switch 10/100Mbit, 100/1000Mbit, with and without PoE support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Script (steam2.sh):&lt;/P&gt;&lt;P&gt;gst-launch-1.0 -v udpsrc port=5002 ! application/x-rtp,payload=96 ! rtph264depay ! queue ! h264parse ! imxvpudec ! imxipuvideosink sync=false window-x-coord=400 window-y-coord=0 window-width=400 window-height=480 force-aspect-ratio=false &amp;amp; &lt;BR /&gt;gst-launch-1.0 -v udpsrc port=10002 ! application/x-rtp,payload=96 ! rtph264depay ! queue ! h264parse ! imxvpudec ! imxipuvideosink sync=false window-x-coord=0 window-y-coord=0 window-width=400 window-height=480 force-aspect-ratio=false&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Camera_Switch.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110012i1B8A41D41A960B35/image-size/large?v=v2&amp;amp;px=999" role="button" title="Camera_Switch.png" alt="Camera_Switch.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is also there when I only show one stream with:&lt;/P&gt;&lt;P&gt;gst-launch-1.0 -v udpsrc port=5002 ! application/x-rtp,payload=96 ! rtph264depay ! queue ! h264parse ! imxvpudec ! imxipuvideosink sync=false force-aspect-ratio=false&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I display CAM_B I will only get a picture here and there. If I display CAM_A everything is okay.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 05:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1083360#M158927</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2020-08-12T05:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: Why do I need a second Switch to receive two streams without judder?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1174429#M164167</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24576"&gt;@MicMoba&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Perhaps the second switch provides additional buffering and this improves performance.&lt;BR /&gt;Please try to increase Gstreamer buffering.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 09:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-do-I-need-a-second-Switch-to-receive-two-streams-without/m-p/1174429#M164167</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-10-28T09:40:47Z</dc:date>
    </item>
  </channel>
</rss>