<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot Issue from EMMC on i.MX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082763#M158837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are investigating a problem related to the start-up of a IMX6Q processor booting from the eMMC&lt;SPAN style="color: #1f497d;"&gt; device&lt;/SPAN&gt;. We have about 20 board&lt;SPAN style="color: #1f497d;"&gt;s&lt;/SPAN&gt; among a lot of 300 pieces that show the same behaviour.&lt;/P&gt;&lt;P&gt;The iMX6Q processor is installed on a custom CPU board. The eMMC &lt;SPAN style="color: #1f497d;"&gt;device &lt;/SPAN&gt;is the SANDISK p.n. SDIN8DE2-4G.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After the power-up the BOOTSEL are correctly sampled and the iMX start the operation in order to identify the eMMC &lt;SPAN style="color: #1f497d;"&gt;device&lt;/SPAN&gt; installed and connected to the SD4 interface.&lt;/P&gt;&lt;P&gt;Following the flowchart of the iMX &amp;nbsp;internal BOOT-ROM, the processor sen&lt;SPAN style="color: #1f497d;"&gt;ds&lt;/SPAN&gt; the CMD0 (GO_IDLE_STATE) command&lt;SPAN style="color: #1f497d;"&gt;, then follows a loop&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;of&lt;/SPAN&gt; the CMD1 command (SEND_OP_COND).&lt;/P&gt;&lt;P&gt;This command is sent until the eMMC sets to logic level 1 the MSB of the OCR register. Then the processor sen&lt;SPAN style="color: #1f497d;"&gt;ds&lt;/SPAN&gt; the CMD2 command in order to identify the eMMC &lt;SPAN style="color: #1f497d;"&gt;device&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;At the end of this command the clk signal driven by the iMX6Q stops and then the processor goes in serial download state waiting for USB connection.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;This Issue is very critical for us and we look forward to receive a feedback as soon as possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 14:18:25 GMT</pubDate>
    <dc:creator>diegobovi85</dc:creator>
    <dc:date>2020-06-10T14:18:25Z</dc:date>
    <item>
      <title>Boot Issue from EMMC on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082763#M158837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are investigating a problem related to the start-up of a IMX6Q processor booting from the eMMC&lt;SPAN style="color: #1f497d;"&gt; device&lt;/SPAN&gt;. We have about 20 board&lt;SPAN style="color: #1f497d;"&gt;s&lt;/SPAN&gt; among a lot of 300 pieces that show the same behaviour.&lt;/P&gt;&lt;P&gt;The iMX6Q processor is installed on a custom CPU board. The eMMC &lt;SPAN style="color: #1f497d;"&gt;device &lt;/SPAN&gt;is the SANDISK p.n. SDIN8DE2-4G.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After the power-up the BOOTSEL are correctly sampled and the iMX start the operation in order to identify the eMMC &lt;SPAN style="color: #1f497d;"&gt;device&lt;/SPAN&gt; installed and connected to the SD4 interface.&lt;/P&gt;&lt;P&gt;Following the flowchart of the iMX &amp;nbsp;internal BOOT-ROM, the processor sen&lt;SPAN style="color: #1f497d;"&gt;ds&lt;/SPAN&gt; the CMD0 (GO_IDLE_STATE) command&lt;SPAN style="color: #1f497d;"&gt;, then follows a loop&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;of&lt;/SPAN&gt; the CMD1 command (SEND_OP_COND).&lt;/P&gt;&lt;P&gt;This command is sent until the eMMC sets to logic level 1 the MSB of the OCR register. Then the processor sen&lt;SPAN style="color: #1f497d;"&gt;ds&lt;/SPAN&gt; the CMD2 command in order to identify the eMMC &lt;SPAN style="color: #1f497d;"&gt;device&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;At the end of this command the clk signal driven by the iMX6Q stops and then the processor goes in serial download state waiting for USB connection.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;This Issue is very critical for us and we look forward to receive a feedback as soon as possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 14:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082763#M158837</guid>
      <dc:creator>diegobovi85</dc:creator>
      <dc:date>2020-06-10T14:18:25Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Issue from EMMC on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082764#M158838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;issue may be related to poor soldering so one can try to resolder&lt;/P&gt;&lt;P&gt;chips. Also one can consider similar issue on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332110"&gt;https://community.nxp.com/thread/332110&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 23:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082764#M158838</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-10T23:02:52Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Issue from EMMC on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082765#M158839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we asked to our contract manufacturer to analyze the PC boards with the emmc issue. They performed an X-ray analysis to check the components soldering quality of the imx6q cpu and emmc device. All the 5 analyzed boards did not have soldering issues. We also tried to change the emmc component, so we removed the SA&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;NDISK SDIN8DE2-4G and we installed the MICRON MTFC4GACAJCN device, but the behavior did not change.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Our problem is not linux related, since it appears at the very beginning during the execution of the imx boot rom code.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 07:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082765#M158839</guid>
      <dc:creator>diegobovi85</dc:creator>
      <dc:date>2020-07-06T07:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Issue from EMMC on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082766#M158840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there any guidelines&amp;nbsp;or constraints to connect the emmc device to the imx6q cpu? I mean, for example, external pull-ups, pull-downs, termination resistors, and so on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 07:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082766#M158840</guid>
      <dc:creator>diegobovi85</dc:creator>
      <dc:date>2020-07-06T07:50:50Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Issue from EMMC on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082767#M158841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example of connection one can look at &amp;nbsp;iMX6Q-SABRE-SDB-DESIGNFILES&lt;/P&gt;&lt;H3 class=""&gt;&lt;A data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emulation)" href="https://www.nxp.com/webapp/Download?colCode=iMX6Q-SABRE-SDB-DESIGNFILES&amp;amp;appType=license"&gt;Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emulation)&lt;/A&gt;&lt;/H3&gt;&lt;P&gt;emmc layout rules in sect.3.6.8 High speed signal routing recommendations&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG" target="_blank"&gt;&lt;STRONG&gt;IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 09:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Issue-from-EMMC-on-i-MX6Q/m-p/1082767#M158841</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-07-06T09:09:45Z</dc:date>
    </item>
  </channel>
</rss>