<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using uuu to load imx8mq eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082458#M158807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My Arrow field engineer helped me discover the uuu_imx_android_flash.sh script in the android build output directory.&lt;/P&gt;&lt;P&gt;I've been messing with it and have made some progress, but now it appears that the eMMC load hangs. I made a couple of changes to the script to accept var-dart et al in order to align it with my build output. I also added -v -V to the uuu args.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the generated uuu.lst file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu_version 1.3.102&lt;BR /&gt;SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f u-boot-imx8mq-var-dart-uuu.imx -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f u-boot-imx8mq-var-dart-uuu.imx -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev 0&lt;BR /&gt;FB: ucmd mmc dev 0&lt;BR /&gt;FB: ucmd mmc dev 0 0&lt;BR /&gt;FB: ucmd mmc erase 0x2000 0x8&lt;BR /&gt;FB: ucmd mmc partconf 0 1 1 1&lt;BR /&gt;FB: flash bootloader0 u-boot-imx8mq-var-dart.imx&lt;BR /&gt;FB: flash gpt partition-table.img&lt;BR /&gt;FB: ucmd setenv fastboot_dev sata&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: flash dtbo_a dtbo-imx8mq-var-dart-sd-hdmi.img&lt;BR /&gt;FB: flash boot_a boot.img&lt;BR /&gt;FB: flash system_a system.img&lt;BR /&gt;FB: flash vendor_a vendor.img&lt;BR /&gt;FB: flash product_a product.img&lt;BR /&gt;FB: flash vbmeta_a vbmeta-imx8mq-var-dart-sd-hdmi.img&lt;BR /&gt;FB[-t 600000]: erase misc&lt;BR /&gt;FB[-t 600000]: erase presistdata&lt;BR /&gt;FB[-t 600000]: erase fbmisc&lt;BR /&gt;FB: set_active a&lt;BR /&gt;FB[-t 600000]: erase userdata&lt;BR /&gt;FB: done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my script call and output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~/var_imx-android-10.0.0_1.0.0/android_build/out/target/product/dart_mx8mq$ sudo ./uuu_imx_android_flash.sh -f imx8mq -a -e -t emmc -u var-dart -d var-dart-sd-hdmi -p var-dart&lt;BR /&gt;This script is validated with uuu 1.3.102 version, please align with this version.&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;generate lines to flash u-boot-imx8mq-var-dart.imx to the partition of bootloader0&lt;BR /&gt;generate lines to flash partition-table.img to the partition of gpt&lt;BR /&gt;generate lines to flash dtbo-imx8mq-var-dart-sd-hdmi.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash system.img to the partition of system_a&lt;BR /&gt;generate lines to flash vendor.img to the partition of vendor_a&lt;BR /&gt;generate lines to flash product.img to the partition of product_a&lt;BR /&gt;generate lines to flash vbmeta-imx8mq-var-dart-sd-hdmi.img to the partition of vbmeta_a&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.154-0-g47ddef5&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt; Pctl Chip Vid Pid BcdVersion&lt;BR /&gt; ==================================================&lt;BR /&gt; SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt; SDPS: MX28 0x15a2 0x004f&lt;BR /&gt; SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt; SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt; SDP: MX7D 0x15a2 0x0076&lt;BR /&gt; SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt; SDP: MX6D 0x15a2 0x0061&lt;BR /&gt; SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt; SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt; SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt; SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt; SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt; SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt; SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt; SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt; SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt; SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt; FBK: 0x066f 0x9afe&lt;BR /&gt; FBK: 0x066f 0x9bff&lt;BR /&gt; FB: 0x0525 0xa4a5&lt;BR /&gt; FB: 0x18d1 0x0d02&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:21&lt;BR /&gt;1:21&amp;gt;Start Cmd:SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx&lt;BR /&gt;6400%1:21&amp;gt;Okay (2.68s)&lt;BR /&gt;^C (I interrupted here after waiting for a while without any signs of progress)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the device console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2019.04-41456-g4de18fd2b7 (Jul 21 2020 - 07:55:47 -0500)&lt;BR /&gt;PMIC: PFUZE100 ID=0x10&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jul 2020 16:39:09 GMT</pubDate>
    <dc:creator>tuban</dc:creator>
    <dc:date>2020-07-24T16:39:09Z</dc:date>
    <item>
      <title>Using uuu to load imx8mq eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082455#M158804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a custom board using an imx8mq Variscite SOM with eMMC only (no SD) and have successfully used uuu to load linux images using uuu, but am having difficulty loading android 10. I see posts for both 'uuu android.zip' and 'uuu-android-mx8mm-evk-emmc.lst', but I do not know how to create android.zip and cannot find the .lst script which I may be able to modify for my situation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--tnx&lt;/P&gt;&lt;P&gt;--tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 13:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082455#M158804</guid>
      <dc:creator>tuban</dc:creator>
      <dc:date>2020-07-23T13:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: Using uuu to load imx8mq eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082456#M158805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for building image one can look at sect.3 Building the Android platform for i.MX &lt;A href="https://www.nxp.com/docs/en/user-guide/ANDROID_USERS_GUIDE.pdf"&gt;Android User’s Guide&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID" title="https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID"&gt;Android OS for i.MX Applications Processors | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 23:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082456#M158805</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-07-23T23:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: Using uuu to load imx8mq eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082457#M158806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for helping on this Igor. Let me explain more of the details. I am able to build the android image set successfully. I have even been able to load built images onto the variscite demo board, which has SD. My problem is loading our custom board which only has eMMC. I am running under Ubuntu, not windows. I have successfully used the uuu tool under Ubuntu to load the linux build onto eMMC (via USB). I see references to being able to either use 'uuu android.zip' to load eMMC via USB and 'uuu uuu-android-mx8mm-evk-emmc.lst'. I believe that if I can find a .lst file example, I can tailor it to our system. Or, if I knew what files to zip together, that may work too. I just don't see instructions for either of these in the documentation or other forum questions. Do I really have to run Windows to do this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 14:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082457#M158806</guid>
      <dc:creator>tuban</dc:creator>
      <dc:date>2020-07-24T14:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using uuu to load imx8mq eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082458#M158807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My Arrow field engineer helped me discover the uuu_imx_android_flash.sh script in the android build output directory.&lt;/P&gt;&lt;P&gt;I've been messing with it and have made some progress, but now it appears that the eMMC load hangs. I made a couple of changes to the script to accept var-dart et al in order to align it with my build output. I also added -v -V to the uuu args.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the generated uuu.lst file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu_version 1.3.102&lt;BR /&gt;SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f u-boot-imx8mq-var-dart-uuu.imx -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f u-boot-imx8mq-var-dart-uuu.imx -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev 0&lt;BR /&gt;FB: ucmd mmc dev 0&lt;BR /&gt;FB: ucmd mmc dev 0 0&lt;BR /&gt;FB: ucmd mmc erase 0x2000 0x8&lt;BR /&gt;FB: ucmd mmc partconf 0 1 1 1&lt;BR /&gt;FB: flash bootloader0 u-boot-imx8mq-var-dart.imx&lt;BR /&gt;FB: flash gpt partition-table.img&lt;BR /&gt;FB: ucmd setenv fastboot_dev sata&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: flash dtbo_a dtbo-imx8mq-var-dart-sd-hdmi.img&lt;BR /&gt;FB: flash boot_a boot.img&lt;BR /&gt;FB: flash system_a system.img&lt;BR /&gt;FB: flash vendor_a vendor.img&lt;BR /&gt;FB: flash product_a product.img&lt;BR /&gt;FB: flash vbmeta_a vbmeta-imx8mq-var-dart-sd-hdmi.img&lt;BR /&gt;FB[-t 600000]: erase misc&lt;BR /&gt;FB[-t 600000]: erase presistdata&lt;BR /&gt;FB[-t 600000]: erase fbmisc&lt;BR /&gt;FB: set_active a&lt;BR /&gt;FB[-t 600000]: erase userdata&lt;BR /&gt;FB: done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my script call and output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~/var_imx-android-10.0.0_1.0.0/android_build/out/target/product/dart_mx8mq$ sudo ./uuu_imx_android_flash.sh -f imx8mq -a -e -t emmc -u var-dart -d var-dart-sd-hdmi -p var-dart&lt;BR /&gt;This script is validated with uuu 1.3.102 version, please align with this version.&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;generate lines to flash u-boot-imx8mq-var-dart.imx to the partition of bootloader0&lt;BR /&gt;generate lines to flash partition-table.img to the partition of gpt&lt;BR /&gt;generate lines to flash dtbo-imx8mq-var-dart-sd-hdmi.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash system.img to the partition of system_a&lt;BR /&gt;generate lines to flash vendor.img to the partition of vendor_a&lt;BR /&gt;generate lines to flash product.img to the partition of product_a&lt;BR /&gt;generate lines to flash vbmeta-imx8mq-var-dart-sd-hdmi.img to the partition of vbmeta_a&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.154-0-g47ddef5&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt; Pctl Chip Vid Pid BcdVersion&lt;BR /&gt; ==================================================&lt;BR /&gt; SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt; SDPS: MX28 0x15a2 0x004f&lt;BR /&gt; SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt; SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt; SDP: MX7D 0x15a2 0x0076&lt;BR /&gt; SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt; SDP: MX6D 0x15a2 0x0061&lt;BR /&gt; SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt; SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt; SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt; SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt; SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt; SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt; SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt; SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt; SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt; SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt; FBK: 0x066f 0x9afe&lt;BR /&gt; FBK: 0x066f 0x9bff&lt;BR /&gt; FB: 0x0525 0xa4a5&lt;BR /&gt; FB: 0x18d1 0x0d02&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:21&lt;BR /&gt;1:21&amp;gt;Start Cmd:SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx&lt;BR /&gt;6400%1:21&amp;gt;Okay (2.68s)&lt;BR /&gt;^C (I interrupted here after waiting for a while without any signs of progress)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the device console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2019.04-41456-g4de18fd2b7 (Jul 21 2020 - 07:55:47 -0500)&lt;BR /&gt;PMIC: PFUZE100 ID=0x10&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 16:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-uuu-to-load-imx8mq-eMMC/m-p/1082458#M158807</guid>
      <dc:creator>tuban</dc:creator>
      <dc:date>2020-07-24T16:39:09Z</dc:date>
    </item>
  </channel>
</rss>