<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDMIC input volume very low</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DMIC-input-volume-very-low/m-p/1082077#M158745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to record voice through the dmic present on my board, the audio codec used is wm8962, the codec provides 1.8v to the dmic and dmic clock runs at 2.8MHz. But, when I record anything through the dmic i am not able to hear anything in the playback.&lt;/P&gt;&lt;P&gt;Kindly help to find a solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anusha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 10:32:34 GMT</pubDate>
    <dc:creator>anushan</dc:creator>
    <dc:date>2020-06-10T10:32:34Z</dc:date>
    <item>
      <title>DMIC input volume very low</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DMIC-input-volume-very-low/m-p/1082077#M158745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to record voice through the dmic present on my board, the audio codec used is wm8962, the codec provides 1.8v to the dmic and dmic clock runs at 2.8MHz. But, when I record anything through the dmic i am not able to hear anything in the playback.&lt;/P&gt;&lt;P&gt;Kindly help to find a solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anusha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 10:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DMIC-input-volume-very-low/m-p/1082077#M158745</guid>
      <dc:creator>anushan</dc:creator>
      <dc:date>2020-06-10T10:32:34Z</dc:date>
    </item>
    <item>
      <title>Re: DMIC input volume very low</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DMIC-input-volume-very-low/m-p/1082078#M158746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anusha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to tweak "attenuation" factor described in Table 7-7. Audio Mixer controls&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux Manual in &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 23:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DMIC-input-volume-very-low/m-p/1082078#M158746</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-10T23:05:10Z</dc:date>
    </item>
  </channel>
</rss>