<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8MM USB2.0 Design Without USB TYPE-C</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-USB2-0-Design-Without-USB-TYPE-C/m-p/1079901#M158469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;I`m designing a new base board using the IMX8MM EVK. i plan to connect a UVC camera directly to USB1 (without a connector).&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i followed the instruction below but i am not sure about IOMUX part, what do i need to change in the device tree?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;A href="https://community.nxp.com/thread/530525"&gt;https://community.nxp.com/thread/530525&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;also, the USB_OTG_ID pin is currently used for the ETH, what do i need to change in order to use the USB_ID instead?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Thanks,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Dudi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 May 2020 05:49:15 GMT</pubDate>
    <dc:creator>dudisasson</dc:creator>
    <dc:date>2020-05-13T05:49:15Z</dc:date>
    <item>
      <title>i.MX8MM USB2.0 Design Without USB TYPE-C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-USB2-0-Design-Without-USB-TYPE-C/m-p/1079901#M158469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;I`m designing a new base board using the IMX8MM EVK. i plan to connect a UVC camera directly to USB1 (without a connector).&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i followed the instruction below but i am not sure about IOMUX part, what do i need to change in the device tree?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;A href="https://community.nxp.com/thread/530525"&gt;https://community.nxp.com/thread/530525&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;also, the USB_OTG_ID pin is currently used for the ETH, what do i need to change in order to use the USB_ID instead?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Thanks,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Dudi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 05:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-USB2-0-Design-Without-USB-TYPE-C/m-p/1079901#M158469</guid>
      <dc:creator>dudisasson</dc:creator>
      <dc:date>2020-05-13T05:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MM USB2.0 Design Without USB TYPE-C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-USB2-0-Design-Without-USB-TYPE-C/m-p/1079902#M158470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dudi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can refer to the document, which is related to your question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-346008"&gt;https://community.nxp.com/docs/DOC-346008&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;B.R,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 07:44:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-USB2-0-Design-Without-USB-TYPE-C/m-p/1079902#M158470</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-05-15T07:44:56Z</dc:date>
    </item>
  </channel>
</rss>