<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6sx: uart6 and rpmsg issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078894#M158354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Angelo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uart6 is listed in Table 4-1. Pin Assignments &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6SXRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6SoloX Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;it is the same as other uarts. For rpmsg issue one can try to reproduce issue&lt;/P&gt;&lt;P&gt;on nxp sabre sd board with official linux from source.codeaurora.org/external/imx/linux-imx&amp;nbsp; repository&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_LINUX_DOCS" target="_blank"&gt;Linux 4.14.98_2.2.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2020 00:40:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-05-28T00:40:55Z</dc:date>
    <item>
      <title>imx6sx: uart6 and rpmsg issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078893#M158353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am on a simple busybox-based&amp;nbsp; rootfs, 4.14 imx-2.0.0 kernel, and observing a strange issue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by a simple bash script, i am performing a simple read / write test from uart2 to uart6, and just after i perform a rpmsg m4 r/w test using the endpoint driver (ept created by echo 1 &amp;gt; /sys/class/rpmsg/channel_1/ept_new), after repeating 4 time the test, rpmsg channel read / write test hangs blocking execution, can exit by CTRL-.Z only and by ps i see rpmsg test process in R state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i remove the test on uart6, test uart2 to 5 + rpmsg works fine forever in a loop.&lt;/P&gt;&lt;P&gt;So seems uart6 has some special connection with rpmsg.&lt;/P&gt;&lt;P&gt;Also, in the imx6sx rm, after "Table 65-6. UART5 External Signals"&amp;nbsp; i don't see any uart6 table, and this make me think uart6 is someway special.&lt;/P&gt;&lt;P&gt;I am going deeper, but if any help, welcome.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 09:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078893#M158353</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2020-05-27T09:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx6sx: uart6 and rpmsg issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078894#M158354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Angelo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uart6 is listed in Table 4-1. Pin Assignments &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6SXRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6SoloX Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;it is the same as other uarts. For rpmsg issue one can try to reproduce issue&lt;/P&gt;&lt;P&gt;on nxp sabre sd board with official linux from source.codeaurora.org/external/imx/linux-imx&amp;nbsp; repository&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_LINUX_DOCS" target="_blank"&gt;Linux 4.14.98_2.2.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 00:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078894#M158354</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-28T00:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx6sx: uart6 and rpmsg issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078895#M158355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks ! I solved, since rpmsg dialog was stuck after touching uart6, i had a look into the m4 firmware, and it is using UART6 as debug uart. So, for my case, even if accessible from cortex-A side should not be touched.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 07:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sx-uart6-and-rpmsg-issue/m-p/1078895#M158355</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2020-05-29T07:37:46Z</dc:date>
    </item>
  </channel>
</rss>