<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx8qxp u-boot spi driver support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077852#M158222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Any chance to review the availability of SPI bus driver in u-boot source ?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2020 11:31:59 GMT</pubDate>
    <dc:creator>rutvij_trivedi</dc:creator>
    <dc:date>2020-08-18T11:31:59Z</dc:date>
    <item>
      <title>imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077847#M158217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I am working with imx8qxp , i am using yocto(sumo) setup with u-boot version imx_v2018.03_4.14.78_1.0.0_ga.&lt;BR /&gt;I want to enable security chip which is using normal SPI interface.&lt;/P&gt;&lt;P&gt;I am able to bring up this IC from kernel using LPSPI.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;When i looked at the u-boot source i was not able find any lpspi driver and below are available drivers in my source tree.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110205iFBF30C53458F8FC8/image-size/large?v=v2&amp;amp;px=999" title="uboot-spi-tree.png" alt="uboot-spi-tree.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So how do i use normal spi bus driver on imx8qxp in u-boot-2018 ?&lt;BR /&gt;&lt;BR /&gt;Any help would be greatly appreciable.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Rutvij&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 07:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077847#M158217</guid>
      <dc:creator>rutvij_trivedi</dc:creator>
      <dc:date>2020-08-10T07:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077848#M158218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can refer to the kernel device tree file:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qxp-lpddr4-arm2-lpspi.dts?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qxp-lpddr4-arm2-lpspi.dts?h=imx_4.14.78_1.0.0_ga"&gt;fsl-imx8qxp-lpddr4-arm2-lpspi.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2020 07:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077848#M158218</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-13T07:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077849#M158219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;BR /&gt;Thank for the reply,&lt;BR /&gt;But i think you should read the question again , as it says "&lt;STRONG&gt;I am able to bring up this IC from kernel using LPSPI&lt;/STRONG&gt;." and the concern is related to u-boot and not the kernel.&lt;BR /&gt;&lt;STRONG&gt;LPSPI driver and its DTS configuration seems not available in the u-boot source(?)&lt;/STRONG&gt;.&lt;BR /&gt;&lt;BR /&gt;So how do i enable imx8qxp LPSPI or normal&amp;nbsp; SPI in &lt;STRONG&gt;u-boot source&lt;/STRONG&gt; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2020 08:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077849#M158219</guid>
      <dc:creator>rutvij_trivedi</dc:creator>
      <dc:date>2020-08-13T08:14:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077851#M158221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks fr the reply.&lt;BR /&gt;As the link suggested, there should be compatible driver available in the same repo, but when looked at it unfortunately i was unable to find the compatible driver here as well as in my repo after switching to the same branch.&lt;BR /&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/spi?h=imx_v2019.04_4.19.35_1.0.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/spi?h=imx_v2019.04_4.19.35_1.0.0"&gt;spi\drivers - uboot-imx - i.MX U-Boot&lt;/A&gt; . (same link provided as above, but directory is driver)&lt;BR /&gt;I could add compatible string in &lt;STRONG&gt;spidev.c&lt;/STRONG&gt; but it also does not seem available &lt;BR /&gt;I could find lpspi driver node in dts file but can not find any compatible &lt;STRONG&gt;"fsl,imx7ulp-spi"&lt;/STRONG&gt; driver in source.&lt;/P&gt;&lt;P&gt;Also the dts file you suggested is for imx8qm devices but i m using &lt;STRONG&gt;imx8qxp,&lt;/STRONG&gt; will this work for both ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Is there anything i am missing here ?&lt;BR /&gt;Can you please verify at your end ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2020 09:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077851#M158221</guid>
      <dc:creator>rutvij_trivedi</dc:creator>
      <dc:date>2020-08-17T09:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077852#M158222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Any chance to review the availability of SPI bus driver in u-boot source ?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 11:31:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077852#M158222</guid>
      <dc:creator>rutvij_trivedi</dc:creator>
      <dc:date>2020-08-18T11:31:59Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp u-boot spi driver support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077853#M158223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got the reply from expert team:&lt;/P&gt;&lt;P&gt;"There is no LSPI driver for 8X/8 in u-boot."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 07:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-u-boot-spi-driver-support/m-p/1077853#M158223</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-26T07:49:34Z</dc:date>
    </item>
  </channel>
</rss>