<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX7D MIPI Display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075772#M157926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm asking about the MIPI display driver, not camera driver. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 May 2020 03:14:36 GMT</pubDate>
    <dc:creator>hellfire3456789</dc:creator>
    <dc:date>2020-05-14T03:14:36Z</dc:date>
    <item>
      <title>IMX7D MIPI Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075770#M157924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I've been trying to setup a MIPI display with Linux on a IMX7Dual Sabre development board and am running into some trouble. I'm using an ST7701 display driver as my chip, which I previously had working on a parallel interface on an IMX6UL. I have ported over all the initilisation parameters so they send using the MIPI interface rather than the SPI interface I was using before. However, when I read from the chip, it returns incorrect data (Reading the chip ID does not return what the data sheets states that it will). It does not time out however.&lt;BR /&gt;&lt;BR /&gt;Looking at the driver (is mipi_dsi_samsung.c the correct driver?) there seems to be a lot magic numbers setting up the PLLs. Is there any need to modify these values for my use case? Is there any guidance as to what they should be?&lt;BR /&gt;&lt;BR /&gt;I also notice the pixel format is hard coded as 24-bit, is there a need to change this to have it function correctly for a 16-bit display?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 08:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075770#M157924</guid>
      <dc:creator>hellfire3456789</dc:creator>
      <dc:date>2020-05-12T08:46:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D MIPI Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075771#M157925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OV5647 mipi camera was verified on iMX7D board.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="395858" data-objecttype="1" href="https://community.nxp.com/thread/395858"&gt;https://community.nxp.com/thread/395858&lt;/A&gt;&lt;/P&gt;&lt;P&gt;also one can use camera module&amp;nbsp;from Boundary Devices&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fboundarydevices.com%2Fproduct%2Fnit6x_5mp_mipi%2F" rel="nofollow" target="_blank"&gt;OV5640 Camera Module for i.MX6 boards&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for documentation one can refer to Chapter 20 MIPI CSI2 Driver&lt;/P&gt;&lt;P&gt;of the&amp;nbsp; Linux reference Manual installed on your BSP documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you need to change to 16 bit the pixel hardcoded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 13:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075771#M157925</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-05-13T13:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D MIPI Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075772#M157926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm asking about the MIPI display driver, not camera driver. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2020 03:14:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075772#M157926</guid>
      <dc:creator>hellfire3456789</dc:creator>
      <dc:date>2020-05-14T03:14:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D MIPI Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075773#M157927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, one can look at description of mipi drivers in Source Code Structure of the Linux Manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2020 13:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075773#M157927</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-05-14T13:53:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D MIPI Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075774#M157928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have solved this problem, the LCDIF driver is buggy as it pulls the settings for the screen after it sets them, so any screen not using default clock values does not function correctly. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My solution was to move the call to mxsfb_dispdrv_init out of the probe function and into the mxsfb_init_fbinfo function. The MIPI display drivers are pretty poorly written in general, most things are hardcoded in instead of taking them from the settings structure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 01:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-MIPI-Display/m-p/1075774#M157928</guid>
      <dc:creator>hellfire3456789</dc:creator>
      <dc:date>2020-05-15T01:16:23Z</dc:date>
    </item>
  </channel>
</rss>