<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 CSI Capture does not work in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074840#M157786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found the issue for HDMI In - I need to set regmap_update_bits(gpr, IOMUXC_GPR13, 0x3F, 0x20); so HDMI works well then.&lt;/P&gt;&lt;P&gt;But the TVP5151 in on CSI1 still does not work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2020 16:34:52 GMT</pubDate>
    <dc:creator>swendt</dc:creator>
    <dc:date>2020-05-12T16:34:52Z</dc:date>
    <item>
      <title>IMX6 CSI Capture does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074839#M157785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a HW with TC358743 HDMI Decoder connected to MIPI-CSI interface and a TVP5150AM connected as 8-Bit parallel device to CSI1. I am running NXP kernel 4.1.15.&lt;/P&gt;&lt;P&gt;I2C setup etc. all works well, also registration in V4L2 etc but if try to capture the stream of either device, the camera_callback function is never called and no buffers are queued, e.g. using gstreamer or v4l2grab.&lt;/P&gt;&lt;P&gt;I can see that there is activity both on MIPI-CSI and on CSI1 as soon as I start streaming but camera_callback s never called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find my device tree file and my kernel config attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way to further debug the IPU why there is no callback executed ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# v4l2grab&amp;nbsp; -o test.jpg -W 640 -H 480&amp;nbsp; -d /dev/video1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MVC: mxc_v4l_open&lt;BR /&gt;&amp;nbsp;&amp;nbsp; device name is Mxc Camera&lt;BR /&gt;End of mxc_v4l_open: v2f pix widthxheight 288 x 352&lt;BR /&gt;End of mxc_v4l_open: crop_bounds widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l_open: crop_defrect widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l_open: crop_current widthxheight 720 x 525&lt;BR /&gt;On Open: Input to ipu size is 720 x 525&lt;BR /&gt;INIT Test Generator&lt;BR /&gt;Selecting video route: route input=0, output=0 =&amp;gt; tvp5150 input=0, opmode=0&lt;BR /&gt;Set video std register to 0.&lt;BR /&gt;Selecting video route: route input=0, output=0 =&amp;gt; tvp5150 input=0, opmode=0&lt;BR /&gt;Set video std register to 0.&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5604&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;BR /&gt;In MVC: mxc_v4l2_g_fmt type=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_g_fmt: v2f pix widthxheight 288 x 352&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_bounds widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_defrect widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_current widthxheight 720 x 525&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5615&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_PARM&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0405602&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c02c564a&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c02c564a&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0405602&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80045626&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_INPUT&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c050561a&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_ENUMINPUT&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445624&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case default or not supported:-1069263324 - 0xC0445624&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c02c563a&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_CROPCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 4014563c&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_CROP&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Cropping Input to ipu size 720 x 525&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5640&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_FMT&lt;BR /&gt;In MVC: mxc_v4l2_s_fmt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type=V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_s_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_bounds widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_defrect widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_current widthxheight 720 x 525&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5605&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_FMT&lt;BR /&gt;In MVC: mxc_v4l2_s_fmt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type=V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_s_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_bounds widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_defrect widthxheight 720 x 525&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_current widthxheight 720 x 525&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5615&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_PARM&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5616&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_PARM&lt;BR /&gt;In mxc_v4l2_s_param&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current capabilities are 1001&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current capturemode is 0&amp;nbsp; change to 0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current framerate is 30&amp;nbsp; change to 30&lt;BR /&gt;ioctl_s_parm TVP5150_OUTPUT_CONTROL_CHIP_ENABLE&lt;BR /&gt;&amp;nbsp;&amp;nbsp; clock_curr=mclk=0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; g_fmt_cap returns widthxheight of input as 720 x 525&lt;BR /&gt;INIT Test Generator&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0145608&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_REQBUFS&lt;BR /&gt;In MVC:mxc_streamoff&lt;BR /&gt;MVC: In mxc_free_frame_buf&lt;BR /&gt;In MVC:mxc_allocate_frame_buf - size=614400&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72500, start=0x76b55000, end=0x76beb000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72600, start=0x76abf000, end=0x76b55000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 40045612&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_STREAMON&lt;BR /&gt;In MVC:mxc_streamon&lt;BR /&gt;UYVY&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_poll&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# gst-launch-1.0 imxv4l2videosrc ! fakesink&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;In MVC: mxc_v4l_open&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; device name is Mxc Camera&lt;BR /&gt;ioctl_g_ifparm&lt;BR /&gt;ioctl_g_ifparm: clock_curr=mclk=27000000&lt;BR /&gt;get_pixelformat: YUV 4:2:2 8-bit (56595559, 1e)&lt;BR /&gt;ioctl_g_fmt_cap: 640x480&lt;BR /&gt;End of mxc_v4l_open: v2f pix widthxheight 288 x 352&lt;BR /&gt;End of mxc_v4l_open: crop_bounds widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l_open: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l_open: crop_current widthxheight 640 x 480&lt;BR /&gt;On Open: Input to ipu size is 640 x 480&lt;BR /&gt;INIT Test Generator&lt;BR /&gt;tc358743_reset: RESET&lt;BR /&gt;power_control: 0&lt;BR /&gt;power_control: 1&lt;BR /&gt;tc_standby: powerdown=0, power_gp=0xfffffffe&lt;BR /&gt;tc358743_minit: capture mode: 0 fps: 60&lt;BR /&gt;tc358743_init_mode rate: 0 mode: 0&lt;BR /&gt;tc358743_software_reset: mask: 0300 freq: 2700&lt;BR /&gt;mipi_reset: mipi_csi2_info:&lt;BR /&gt;mipi_en:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;BR /&gt;datatype:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 30&lt;BR /&gt;dphy_clk:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; d81d3e80&lt;BR /&gt;pixel_clk:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; d81d3f00&lt;BR /&gt;mipi_csi2_base:f008a000&lt;BR /&gt;pdev:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; d818a200&lt;BR /&gt;Now Using 1 lanes&lt;BR /&gt;tc358743_software_reset: mask: 0200 freq: 2700&lt;BR /&gt;get_pixelformat: YUV 4:2:2 8-bit (56595559, 1e)&lt;BR /&gt;set_frame_rate_mode: Set 44 regs from 80729100 for frs 0 mode 0 with width 640 height 480&lt;BR /&gt;Activate EDID&lt;BR /&gt;MIPICSI2_PHY_STATUS: 300&lt;BR /&gt;0&amp;nbsp; mipi csi2 dphy status 300&lt;BR /&gt;0&amp;nbsp; mipi csi2 err1 0&lt;BR /&gt;ioctl_init&lt;BR /&gt;ioctl_dev_init&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 8008563f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case default or not supported:-2146937281 - 0x8008563F&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80085617&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;BR /&gt;In mxc_v4l2_g_std&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 40085618&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_STD&lt;BR /&gt;In mxc_v4l2_s_std 0&lt;BR /&gt;ERROR: unrecognized std! 0 (PAL=ff, NTSC=b000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5604&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;BR /&gt;In MVC: mxc_v4l2_g_fmt type=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_g_fmt: v2f pix widthxheight 288 x 352&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_bounds widthxheight 720 x 625&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_current widthxheight 720 x 576&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c02c564a&lt;BR /&gt;ioctl_enum_framesizes, mode: 0&lt;BR /&gt;get_pixelformat: YUV 4:2:2 8-bit (56595559, 1e)&lt;BR /&gt;ioctl_enum_framesizes 640:480 format: 56595559&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0045627&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_INPUT&lt;BR /&gt;In MVC:mxc_streamoff&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5616&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_PARM&lt;BR /&gt;In mxc_v4l2_s_param&lt;BR /&gt;ioctl_g_parm type: 1&lt;BR /&gt;ioctl_g_parm done 0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current capabilities are 1001&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current capturemode is 0&amp;nbsp; change to 0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Current framerate is 60&amp;nbsp; change to 30&lt;BR /&gt;ioctl_s_parm&lt;BR /&gt;power_control: 1&lt;BR /&gt;ioctl_g_ifparm&lt;BR /&gt;ioctl_g_ifparm: clock_curr=mclk=27000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; clock_curr=mclk=27000000&lt;BR /&gt;get_pixelformat: YUV 4:2:2 8-bit (56595559, 1e)&lt;BR /&gt;ioctl_g_fmt_cap: 640x480&lt;BR /&gt;&amp;nbsp;&amp;nbsp; g_fmt_cap returns widthxheight of input as 640 x 480&lt;BR /&gt;INIT Test Generator&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5605&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_FMT&lt;BR /&gt;In MVC: mxc_v4l2_s_fmt&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type=V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_s_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_bounds widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_s_fmt: crop_current widthxheight 640 x 480&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5604&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;BR /&gt;In MVC: mxc_v4l2_g_fmt type=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_g_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_bounds widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_current widthxheight 640 x 480&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c008561c&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_CTRL&lt;BR /&gt;In MVC:mxc_v4l2_s_ctrl&lt;BR /&gt;&amp;nbsp;&amp;nbsp; default case&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c008561c&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_CTRL&lt;BR /&gt;In MVC:mxc_v4l2_s_ctrl&lt;BR /&gt;&amp;nbsp;&amp;nbsp; default case&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c008561b&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_CTRL&lt;BR /&gt;In MVC:mxc_v4l2_g_ctrl&lt;BR /&gt;ERROR: v4l2 capture: unsupported ioctrl!&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c008561c&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_S_CTRL&lt;BR /&gt;In MVC:mxc_v4l2_s_ctrl&lt;BR /&gt;&amp;nbsp;&amp;nbsp; default case&lt;BR /&gt;Pipeline is live and does not neeIn MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5604&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;BR /&gt;d PREROLL ...&lt;BR /&gt;In MVC: mxc_v4l2_g_fmt type=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;Setting pipeline to PLAYING ...End of mxc_v4l2_g_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_bounds widthxheight 640 x 480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;New clock: GstSystemClock&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_current widthxheight 640 x 480&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0cc5604&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;BR /&gt;In MVC: mxc_v4l2_g_fmt type=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;BR /&gt;End of mxc_v4l2_g_fmt: v2f pix widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_bounds widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_defrect widthxheight 640 x 480&lt;BR /&gt;End of mxc_v4l2_g_fmt: crop_current widthxheight 640 x 480&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0145608&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_REQBUFS&lt;BR /&gt;In MVC:mxc_streamoff&lt;BR /&gt;MVC: In mxc_free_frame_buf&lt;BR /&gt;In MVC:mxc_allocate_frame_buf - size=614400&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72500, start=0x75469000, end=0x754ff000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72600, start=0x7526a000, end=0x75300000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72800, start=0x751d4000, end=0x7526a000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72900, start=0x7513e000, end=0x751d4000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72b00, start=0x750a8000, end=0x7513e000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_mmap&lt;BR /&gt;&amp;nbsp;&amp;nbsp; pgoff=0x72c00, start=0x75012000, end=0x750a8000&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445609&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;BR /&gt;In MVC:mxc_v4l2_buffer_status&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 80685600&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c044560f&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 40045612&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_STREAMON&lt;BR /&gt;In MVC:mxc_streamon&lt;BR /&gt;MIPICSI2_ENABLE PIXCLK&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c0445611&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;BR /&gt;In MVC:mxc_v4l_dqueue&lt;BR /&gt;ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0&lt;BR /&gt;ERROR: from element /GstPipeline:In MVC:mxc_v4l_ioctl&lt;BR /&gt;pipeline0/GstImxV4l2VideoSrc:imxvIn MVC: mxc_v4l_do_ioctl c008561c&lt;BR /&gt;4l2videosrc0: Internal data strea&amp;nbsp;&amp;nbsp; case VIDIOC_S_CTRL&lt;BR /&gt;m error.&lt;BR /&gt;In MVC:mxc_v4l2_s_ctrl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gstbasesrc.c(3055): gst_base_src&amp;nbsp;&amp;nbsp; default case&lt;BR /&gt;_loop (): /GstPipeline:pipeline0/In MVC:mxc_v4l_ioctl&lt;BR /&gt;GstImxV4l2VideoSrc:imxv4l2videosrIn MVC: mxc_v4l_do_ioctl c008561c&lt;BR /&gt;c0:&lt;BR /&gt;streaming stopped, reason er&amp;nbsp;&amp;nbsp; case VIDIOC_S_CTRL&lt;BR /&gt;ror (-5)&lt;BR /&gt;Execution ended after 0In MVC:mxc_v4l2_s_ctrl&lt;BR /&gt;:00:10.376569001&lt;BR /&gt;Setting pipelin&amp;nbsp;&amp;nbsp; default case&lt;BR /&gt;e to PAUSED ...&lt;BR /&gt;Setting pipelineIn MVC:mxc_v4l_ioctl&lt;BR /&gt;&amp;nbsp;to READY ...&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl c008561b&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_G_CTRL&lt;BR /&gt;In MVC:mxc_v4l2_g_ctrl&lt;BR /&gt;ERROR: v4l2 capture: unsupported ioctrl!&lt;BR /&gt;In MVC:mxc_v4l_ioctl&lt;BR /&gt;In MVC: mxc_v4l_do_ioctl 40045613&lt;BR /&gt;&amp;nbsp;&amp;nbsp; case VIDIOC_STREAMOFF&lt;BR /&gt;In MVC:mxc_streamoff&lt;BR /&gt;In MVC:mxc_free_frames&lt;BR /&gt;In MVC:mxc_v4l_close&lt;BR /&gt;power_control: 0&lt;BR /&gt;tc_standby: powerdown=1, power_gp=0xfffffffe&lt;BR /&gt;mxc_v4l_close: release resource&lt;BR /&gt;MVC: In mxc_free_frame_buf&lt;BR /&gt;In MVC:mxc_free_frames&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 08:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074839#M157785</guid>
      <dc:creator>swendt</dc:creator>
      <dc:date>2020-05-12T08:04:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CSI Capture does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074840#M157786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found the issue for HDMI In - I need to set regmap_update_bits(gpr, IOMUXC_GPR13, 0x3F, 0x20); so HDMI works well then.&lt;/P&gt;&lt;P&gt;But the TVP5151 in on CSI1 still does not work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 16:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074840#M157786</guid>
      <dc:creator>swendt</dc:creator>
      <dc:date>2020-05-12T16:34:52Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CSI Capture does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074841#M157787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for TVP5151 one can look at&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/compulab-yokneam/imx6/blob/master/m6/kernel_imx/0061-ARM-i.MX6-tvp5150-add-tvp5150-video-decoder-support.patch" title="https://github.com/compulab-yokneam/imx6/blob/master/m6/kernel_imx/0061-ARM-i.MX6-tvp5150-add-tvp5150-video-decoder-support.patch"&gt;imx6/0061-ARM-i.MX6-tvp5150-add-tvp5150-video-decoder-support.patch at master · compulab-yokneam/imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also instead "imxv4l2videosrc" community gstreamer-imx plugin one can try&lt;/P&gt;&lt;P&gt;nxp imx-gst1.0-plugins described in Linux Guide found in linux documentation on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW" title="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW"&gt;i.MX Software and Development Tools | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 23:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074841#M157787</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-12T23:24:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CSI Capture does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074842#M157788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Igor.&lt;/P&gt;&lt;P&gt;Hi, actually I am using exactly this driver but as mentioned the camera_callback is never called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 09:07:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074842#M157788</guid>
      <dc:creator>swendt</dc:creator>
      <dc:date>2020-05-13T09:07:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CSI Capture does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074843#M157789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can test with mxc_v4l2_tvin.c from unit tests&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz" title="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz"&gt;http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 11:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CSI-Capture-does-not-work/m-p/1074843#M157789</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-13T11:28:42Z</dc:date>
    </item>
  </channel>
</rss>