<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow do i see USB_OTG enabled device files in linux-imx?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-i-see-USB-OTG-enabled-device-files-in-linux-imx/m-p/1073037#M157578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using yocto sumo version linux kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I enabled the following OTG configuation in menuconfig:&lt;/P&gt;&lt;P&gt;/********************************************************&lt;/P&gt;&lt;P&gt;Symbol: USB_OTG [=y] x&lt;BR /&gt; x Type : boolean x&lt;BR /&gt; x Prompt: OTG support x&lt;BR /&gt; x Location: x&lt;BR /&gt; x -&amp;gt; Device Drivers x&lt;BR /&gt; x -&amp;gt; USB support (USB_SUPPORT [=y]) x&lt;BR /&gt; x (8) -&amp;gt; Support for Host-side USB (USB [=y]) x&lt;BR /&gt; x Defined at drivers/usb/core/Kconfig:44&lt;/P&gt;&lt;P&gt;**********************************************************/&lt;/P&gt;&lt;P&gt;1. What is the device file i can expect in the rootfs with the above change?&lt;/P&gt;&lt;P&gt;2. What are the usb device files needed for communicating with MFG/UUU tool and how do i enable that in the kernel(I see /dev/utp missing)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Anush D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/fsl_utp/tg-p"&gt;#fsl_utp&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/usb_otg/tg-p"&gt;#usb_otg&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/mfgtools/tg-p"&gt;#mfgtools&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/yocto sumo/tg-p"&gt;#yocto sumo&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jul 2020 11:23:29 GMT</pubDate>
    <dc:creator>anush_deekonda</dc:creator>
    <dc:date>2020-07-07T11:23:29Z</dc:date>
    <item>
      <title>How do i see USB_OTG enabled device files in linux-imx?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-i-see-USB-OTG-enabled-device-files-in-linux-imx/m-p/1073037#M157578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using yocto sumo version linux kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I enabled the following OTG configuation in menuconfig:&lt;/P&gt;&lt;P&gt;/********************************************************&lt;/P&gt;&lt;P&gt;Symbol: USB_OTG [=y] x&lt;BR /&gt; x Type : boolean x&lt;BR /&gt; x Prompt: OTG support x&lt;BR /&gt; x Location: x&lt;BR /&gt; x -&amp;gt; Device Drivers x&lt;BR /&gt; x -&amp;gt; USB support (USB_SUPPORT [=y]) x&lt;BR /&gt; x (8) -&amp;gt; Support for Host-side USB (USB [=y]) x&lt;BR /&gt; x Defined at drivers/usb/core/Kconfig:44&lt;/P&gt;&lt;P&gt;**********************************************************/&lt;/P&gt;&lt;P&gt;1. What is the device file i can expect in the rootfs with the above change?&lt;/P&gt;&lt;P&gt;2. What are the usb device files needed for communicating with MFG/UUU tool and how do i enable that in the kernel(I see /dev/utp missing)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Anush D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/fsl_utp/tg-p"&gt;#fsl_utp&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/usb_otg/tg-p"&gt;#usb_otg&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/mfgtools/tg-p"&gt;#mfgtools&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/yocto sumo/tg-p"&gt;#yocto sumo&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 11:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-i-see-USB-OTG-enabled-device-files-in-linux-imx/m-p/1073037#M157578</guid>
      <dc:creator>anush_deekonda</dc:creator>
      <dc:date>2020-07-07T11:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: How do i see USB_OTG enabled device files in linux-imx?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-i-see-USB-OTG-enabled-device-files-in-linux-imx/m-p/1073038#M157579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you want to build the firmware for mfgtool, please refer to this thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/1042399"&gt;https://community.nxp.com/message/1042399&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 08:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-i-see-USB-OTG-enabled-device-files-in-linux-imx/m-p/1073038#M157579</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2020-07-08T08:08:40Z</dc:date>
    </item>
  </channel>
</rss>