<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can someone provide documentation for using the RPMsg-Lite with Android configuration for imx8mn? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-someone-provide-documentation-for-using-the-RPMsg-Lite-with/m-p/1071478#M157373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the iMX8 Nano Evaluation Board. I have downloaded the MCUExpresso SDK for testing out certain applications for the M7 core. I want to use the RPMsg-Lite for communication between the A53 and M7. As per my understanding the applications provided in the SDK are for Linux Configurations. I am looking to have the A53 core running Android and not Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is there documentation available for the RPMsg-Lite to be used for an Android configuration? If yes, can someone provide me the links for the same?&lt;/P&gt;&lt;P&gt;2. If possible can the SDK code be converted for a Android configuration from a for Linux configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TIA,&lt;/P&gt;&lt;P&gt;Anurag&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Aug 2020 05:49:08 GMT</pubDate>
    <dc:creator>anurag16doshi</dc:creator>
    <dc:date>2020-08-27T05:49:08Z</dc:date>
    <item>
      <title>Can someone provide documentation for using the RPMsg-Lite with Android configuration for imx8mn?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-someone-provide-documentation-for-using-the-RPMsg-Lite-with/m-p/1071478#M157373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the iMX8 Nano Evaluation Board. I have downloaded the MCUExpresso SDK for testing out certain applications for the M7 core. I want to use the RPMsg-Lite for communication between the A53 and M7. As per my understanding the applications provided in the SDK are for Linux Configurations. I am looking to have the A53 core running Android and not Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is there documentation available for the RPMsg-Lite to be used for an Android configuration? If yes, can someone provide me the links for the same?&lt;/P&gt;&lt;P&gt;2. If possible can the SDK code be converted for a Android configuration from a for Linux configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TIA,&lt;/P&gt;&lt;P&gt;Anurag&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 05:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-someone-provide-documentation-for-using-the-RPMsg-Lite-with/m-p/1071478#M157373</guid>
      <dc:creator>anurag16doshi</dc:creator>
      <dc:date>2020-08-27T05:49:08Z</dc:date>
    </item>
    <item>
      <title>Re: Can someone provide documentation for using the RPMsg-Lite with Android configuration for imx8mn?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-someone-provide-documentation-for-using-the-RPMsg-Lite-with/m-p/1071479#M157374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have no such examples for Android. Sorry for the inconvenience.&lt;BR /&gt;We only suggest you to refer the documents like this as a reference:&lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-343113" target="test_blank"&gt;https://community.nxp.com/docs/DOC-343113&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 02:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-someone-provide-documentation-for-using-the-RPMsg-Lite-with/m-p/1071479#M157374</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-08-28T02:20:02Z</dc:date>
    </item>
  </channel>
</rss>