<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using DHCP but there is no DHCP server ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-DHCP-but-there-is-no-DHCP-server/m-p/225026#M15733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably best to put ip=none as kernel parameter, and then in startup script run dhcp client and if it fails set up ip address statically.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2013 09:36:39 GMT</pubDate>
    <dc:creator>VladanJovanovic</dc:creator>
    <dc:date>2013-01-15T09:36:39Z</dc:date>
    <item>
      <title>Using DHCP but there is no DHCP server ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-DHCP-but-there-is-no-DHCP-server/m-p/225025#M15732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My platform is i.MX535 running Linux which is generated by LTIB from Freescale. &lt;/P&gt;&lt;P&gt;The platform boots with DHCP setting in U-boot.&lt;/P&gt;&lt;P&gt;If there is a DHCP server, then everything is fine. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;P&gt;If there is no DHCP server, how to automatically revert to static IP?&lt;/P&gt;&lt;P&gt;Is there any setting or configuration available in u-boot, or Linux to achieve that, or I have to write a program to detect that and do the IP setting on my own?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 03:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-DHCP-but-there-is-no-DHCP-server/m-p/225025#M15732</guid>
      <dc:creator>UnisvrTim</dc:creator>
      <dc:date>2013-01-15T03:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: Using DHCP but there is no DHCP server ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-DHCP-but-there-is-no-DHCP-server/m-p/225026#M15733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably best to put ip=none as kernel parameter, and then in startup script run dhcp client and if it fails set up ip address statically.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2013 09:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-DHCP-but-there-is-no-DHCP-server/m-p/225026#M15733</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-01-15T09:36:39Z</dc:date>
    </item>
  </channel>
</rss>