<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: which instruction set shall I use for Cortex-a7</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/which-instruction-set-shall-I-use-for-Cortex-a7/m-p/1071042#M157321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By default A-cores are running in "normal" instruction set not "thumb" one. So you need to use -marm option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Aug 2020 03:50:42 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-08-07T03:50:42Z</dc:date>
    <item>
      <title>which instruction set shall I use for Cortex-a7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-instruction-set-shall-I-use-for-Cortex-a7/m-p/1071041#M157320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;We are using i.mx6ultralite processor module in our project. A yocto build system was used to build linux image. By setting ARM_INSTRUCTION_SET, I can decide which instruction set to be used during compilation.&lt;/P&gt;&lt;P&gt;But I have no idea which one of the two instruction sets (-mthumb or -marm) is better for the processor module.&lt;/P&gt;&lt;P&gt;Can you give me some suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Pan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 18:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-instruction-set-shall-I-use-for-Cortex-a7/m-p/1071041#M157320</guid>
      <dc:creator>panli</dc:creator>
      <dc:date>2020-08-06T18:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: which instruction set shall I use for Cortex-a7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-instruction-set-shall-I-use-for-Cortex-a7/m-p/1071042#M157321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By default A-cores are running in "normal" instruction set not "thumb" one. So you need to use -marm option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 03:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-instruction-set-shall-I-use-for-Cortex-a7/m-p/1071042#M157321</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-08-07T03:50:42Z</dc:date>
    </item>
  </channel>
</rss>