<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8QXP+MAX9286 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069842#M157150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi George&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to allocate more memory in dts file with "reserved-memory":&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.3_2.0.0"&gt;imx8x-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 May 2020 23:24:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-05-25T23:24:24Z</dc:date>
    <item>
      <title>i.MX8QXP+MAX9286</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069841#M157149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now,our customer is use i.MX8QXP L4.14.98 +SerDes MAX9286+MAX96705+Sensor AR1043 as Sourding 360 solution.&lt;/P&gt;&lt;P&gt;MAX9286 and MAX96705 should be found and initial is ok.But:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;E&lt;EM&gt;rror:write reg error:reg=0x3024,val=0x1.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;mxc_isi_souce_fmt_init,set remote fmt fail!&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Error: V4l2src0:Failed to allocate require memey.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So any advise for the problem?&lt;/P&gt;&lt;P&gt;&lt;EM&gt;TKs!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MAX9286-mipi.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107526iD4D3C4CD489B7E81/image-size/large?v=v2&amp;amp;px=999" role="button" title="MAX9286-mipi.jpg" alt="MAX9286-mipi.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="V4L2SRC0.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107527i8D4108DA9001376C/image-size/large?v=v2&amp;amp;px=999" role="button" title="V4L2SRC0.jpg" alt="V4L2SRC0.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 14:11:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069841#M157149</guid>
      <dc:creator>lizboxy</dc:creator>
      <dc:date>2020-05-25T14:11:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP+MAX9286</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069842#M157150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi George&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to allocate more memory in dts file with "reserved-memory":&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.3_2.0.0"&gt;imx8x-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 23:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069842#M157150</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-25T23:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP+MAX9286</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069843#M157151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You use AR1043 sensor，but your driver seems OV10635 sensor，so your remote device camera init failed.&lt;/P&gt;&lt;P&gt;Maybe you should config the driver for AR1043.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 09:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-MAX9286/m-p/1069843#M157151</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2020-06-04T09:53:49Z</dc:date>
    </item>
  </channel>
</rss>