<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6/imx7 uart overrun</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069555#M157123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;BR /&gt;When I use the serial port to send and receive data on imx6d and imx7d, an overrun error occurs when the serial port is sent. The Linux version I use on imx6 is 3.14.52, and the Linux version used on imx7 is 4.9.88.&lt;BR /&gt;Reading the previous post, I found that the serial port has overrun problems. Others have also encountered them. After referring to their previous solutions, I found that it did not solve my problem. For example, remove:&lt;BR /&gt;dev_err(sport-&amp;gt;port.dev, "Rx FIFO overrun\n");&lt;BR /&gt;Use dma.&lt;BR /&gt;When I use serial port to transmit data on IMX6/IMX7, I use dma for data transmission. However, overrun still occurs. Does the official website have a correct solution for this error? Please explain in detail the cause of overrun. I already know that the serial port is too late to receive data and cause an overrun error. What I want to know is where it is too late to receive.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2020 13:45:35 GMT</pubDate>
    <dc:creator>864535720</dc:creator>
    <dc:date>2020-07-21T13:45:35Z</dc:date>
    <item>
      <title>imx6/imx7 uart overrun</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069555#M157123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;BR /&gt;When I use the serial port to send and receive data on imx6d and imx7d, an overrun error occurs when the serial port is sent. The Linux version I use on imx6 is 3.14.52, and the Linux version used on imx7 is 4.9.88.&lt;BR /&gt;Reading the previous post, I found that the serial port has overrun problems. Others have also encountered them. After referring to their previous solutions, I found that it did not solve my problem. For example, remove:&lt;BR /&gt;dev_err(sport-&amp;gt;port.dev, "Rx FIFO overrun\n");&lt;BR /&gt;Use dma.&lt;BR /&gt;When I use serial port to transmit data on IMX6/IMX7, I use dma for data transmission. However, overrun still occurs. Does the official website have a correct solution for this error? Please explain in detail the cause of overrun. I already know that the serial port is too late to receive data and cause an overrun error. What I want to know is where it is too late to receive.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 13:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069555#M157123</guid>
      <dc:creator>864535720</dc:creator>
      <dc:date>2020-07-21T13:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx6/imx7 uart overrun</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069556#M157124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;Please disable busfreq, set cpu to performance mode, and disable deep idle by below command.&lt;/P&gt;&lt;P&gt;echo 0 &amp;gt; /sys/devices/soc0/soc/soc\:busfreq/enable&lt;/P&gt;&lt;P&gt;echo performance &amp;gt; /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor&lt;/P&gt;&lt;P&gt;echo 1 &amp;gt; /sys/devices/system/cpu/cpu0/cpuidle/state1/disable&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need these patches for overrun issue in 3.14.52 however those overrun is fixed in latest bsp, try to upgrade.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 13:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069556#M157124</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-07-22T13:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx6/imx7 uart overrun</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069557#M157125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Bio_TICFSL，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I am on Linux 4.9.88 version, there will be overrun. What should I do with this version?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 08:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-imx7-uart-overrun/m-p/1069557#M157125</guid>
      <dc:creator>864535720</dc:creator>
      <dc:date>2020-07-23T08:26:29Z</dc:date>
    </item>
  </channel>
</rss>