<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: stereo camera using IMX8 mini board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067882#M156913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;gor,&lt;BR /&gt;&lt;BR /&gt;Thanks for the information. I think I found the root cause is that the USB ports on IMX8 Mini board are 2.0 type-C connectors. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;So that's why IMX8 Mini board don't have enough bandwidth to load&amp;nbsp;&lt;SPAN&gt;stereo camera oCamS-1CGN-U&amp;nbsp;which use USB 3.0 port.&lt;BR /&gt;&lt;BR /&gt;I tested this camera with USB 2.0 port on laptop, the same results happen.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Anyway thank you for your kindly support.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Hiep&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2020 04:38:43 GMT</pubDate>
    <dc:creator>hiep_nguyen</dc:creator>
    <dc:date>2020-05-15T04:38:43Z</dc:date>
    <item>
      <title>stereo camera using IMX8 mini board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067880#M156911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Supporters,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm testing stereo camera oCamS-1CGN-U on IMX8 mini board. This camera supports highest resolution is 1280x960 at 45 fps. However I use v4l2-ctl tools to check valid image&amp;nbsp;format, the highest resolution supports 640x480.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# v4l2-ctl -d /dev/video1 --list-formats-ext&lt;BR /&gt;ioctl: VIDIOC_ENUM_FMT&lt;BR /&gt; Type: Video Capture&lt;/P&gt;&lt;P&gt;[0]: 'YUYV' (YUYV 4:2:2)&lt;BR /&gt; Size: Discrete 640x480&lt;BR /&gt; Interval: Discrete 0.022s (45.000 fps)&lt;BR /&gt; Interval: Discrete 0.033s (30.000 fps)&lt;BR /&gt; Interval: Discrete 0.040s (25.000 fps)&lt;BR /&gt; Interval: Discrete 0.050s (20.000 fps)&lt;BR /&gt; Interval: Discrete 0.067s (15.000 fps)&lt;BR /&gt; Interval: Discrete 0.100s (10.000 fps)&lt;BR /&gt; Size: Discrete 640x360&lt;BR /&gt;...&lt;BR /&gt; Size: Discrete 320x240&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to set resolution 1280x960&amp;nbsp; using V4L2 library but it failed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Check with Logitech C920 camera,&amp;nbsp;&lt;SPAN&gt;the highest resolution is same as their specs&lt;/SPAN&gt;, 1920x1080 and also on Ubuntu machine, the oCamS camera work same as their specs, 1280x960.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My doubt is that the IMX8 mini only supports 1 camera, so&amp;nbsp;its bandwidth don't enough to load the stereo camera, hence the highest resolution is cut down.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Did you meet this kind of issue before ? Is my doubt right ? Could you guide me solve this issue ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Hiep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2020 05:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067880#M156911</guid>
      <dc:creator>hiep_nguyen</dc:creator>
      <dc:date>2020-05-11T05:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: stereo camera using IMX8 mini board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067881#M156912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hiep&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right, i.MX8M Mini has one MIPI-CSI compared with two for i.MX8MQ :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf" title="https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MINISASTOCSI daughter card (OV5640) can reach up to 2592x1944@15fps resolution.&lt;/P&gt;&lt;P&gt;One can test it using fsl-imx8mm-evk.dtb in combination with the pipeline below:&lt;BR /&gt;$ gst-launch1.0 v4l2src device=/dev/video0 ! autovideosink&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8-series-accessory-boards:i.MX8-ACCESSORY-BOARDS" title="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8-series-accessory-boards:i.MX8-ACCESSORY-BOARDS"&gt;i.MX 8 Series Accessory Boards | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Support for other cameras should be added according to Linux documentation available on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW" title="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW"&gt;i.MX Software and Development Tools | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2020 11:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067881#M156912</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-11T11:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: stereo camera using IMX8 mini board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067882#M156913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;gor,&lt;BR /&gt;&lt;BR /&gt;Thanks for the information. I think I found the root cause is that the USB ports on IMX8 Mini board are 2.0 type-C connectors. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;So that's why IMX8 Mini board don't have enough bandwidth to load&amp;nbsp;&lt;SPAN&gt;stereo camera oCamS-1CGN-U&amp;nbsp;which use USB 3.0 port.&lt;BR /&gt;&lt;BR /&gt;I tested this camera with USB 2.0 port on laptop, the same results happen.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Anyway thank you for your kindly support.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Hiep&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 04:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stereo-camera-using-IMX8-mini-board/m-p/1067882#M156913</guid>
      <dc:creator>hiep_nguyen</dc:creator>
      <dc:date>2020-05-15T04:38:43Z</dc:date>
    </item>
  </channel>
</rss>